Skip to main content
Tyto _Negro_
Associate
January 26, 2018
Question

RTC periodic wake up interrupt fires only once

  • January 26, 2018
  • 2 replies
  • 940 views
Posted on January 26, 2018 at 21:05

Hi, I'm writing an application with a STM32L051 (32 pin, 64kB ROM).

This application uses the RTC and I wanted to use the RTC periodic auto wake-up feature to update the time display every 60 seconds.

THE PROBLEM:

It looks like the interrupt only happens once at the expected time: after 60 seconds (or any other value I tried)

I found an other person having the same problem on a L053 processor using HAL libraries, but no answer or solution was presented. I don't use HAL libraries.

My interrupt code looks like this:

void RTC_IRQHandler(void)
{
 // when Intr. pending
 if ((EXTI->PR & EXTI_PR_PIF20) == EXTI_PR_PIF20){
 RTC->ISR &= ~(RTC_ISR_WUTWF); // CLR Wake Up intr. flag
 EXTI->PR |= EXTI_PR_PIF20; // CLR intr. pending flag (Write 1)
 secs = 0;
 GetTimeDate();
 if ( BTF(KlokStat,klok_on) || BTF(KlokStat,sleep) ){
 DisplayTime(hrs,mins);
 }
 // the 4 lines below were all to test for a solution, to no avail...
 RTC->CR = RTC_CR_WUTE | RTC_CR_WUTIE;
 NVIC_ClearPendingIRQ(RTC_IRQn); // CLR intr pending register
 EXTI->IMR |= EXTI_IMR_IM20; // re-enable RTC wake-up intr. 
 NVIC_EnableIRQ(RTC_IRQn); // Re-eanble NVIC for RTC */
 }
}

The RTC wake-up initialisation code:

/* RTC init function */
static void MX_RTC_Init(void)
{
 RTC->WPR = 0xCA; // Unlock Write access for RTC registers
 RTC->WPR = 0x53;
 RTC->CR &= ~RTC_CR_WUTE; // Disable wake up timer to modify it
 // Wait until it is allow to modify wake up reload value
 while((RTC->ISR & RTC_ISR_WUTWF) != RTC_ISR_WUTWF)
 {
 /* add time out here for a robust application */
 } 
 RTC->WUTR = 0x3B; // wake-up period = 60 sec. 0x3B=59

 // enable WU tmr, WU tmr Intr. and WU clk =1Hz
 RTC->CR = RTC_CR_WUTE | RTC_CR_WUTIE | RTC_CR_WUCKSEL_2;
 RTC->WPR = 0xFE; // write protect/lock again
 RTC->WPR = 0x64;
 EXTI->RTSR |= EXTI_RTSR_RT20; // trigger on rising edge
 // EXTI->FTSR |= EXTI_FTSR_FT20; // no trigger on falling edge
 EXTI->IMR |= EXTI_IMR_IM20; // enable RTC wake-up intr. going through EXTI 20 line to NVIC
 //EXTI->EMR |= EXTI_IMR_IM20; // enable RTC wake-up event necessary?????????

 NVIC_EnableIRQ(RTC_IRQn); // Configure NVIC for RTC
 NVIC_SetPriority(RTC_IRQn,2); // Set priority for RTC (=2, low priority)

}

My application does *not* sleep, so no real 'wake up' things, I just want to use the interrupt routine to update the clock.

I'm also confused by the interrupt/event thing, but enabling the EXTI event does not make any difference.

Any help or tips are highly appreciated.

Thanks, Tom

#once #stm32l0x #wake-up #rtc #interrupt
This topic has been closed for replies.

2 replies

Konami
Senior
October 25, 2018

Any solution to this?

WPuch
Associate III
June 5, 2019

Did you find any solution for that problem? I have exactly the same problem with STM32L452RE. Initialize wakeup times exactly the same way, and get exactly the same result as you. Just one interrupt and that's all.