Thanks for this info. This should be very useful.
The define ...RTCEN you provided is close to what I was looking for, but I originally could only find defines of "...RTCEN" that were 0x1 not 0x1<<15. This would make coding extreeemely cumbersome so I defined my own. I will have to revisit that since you've shown me they do exist. However, a second reason I defined my own is I don't like to type "_" plus the value RTCEN must be used in RCC->BDCR. As I already know the constant is used in that register, why do I want to type "RCC_BCDR_" every time I use "RTCEN"? So I defined my own that are the short version of the bit name. And I wanted the constant to explicitly say what I am doing, hence RTCENon and RTCENoff.
That I was only setting the _S was a mistake. When I was writing my first response, I found several issues with my code that I have corrected, that one in particular had a visible affect. That was why the RTC was running very fast.
Using an actual complete BCD number instead of the separated BCD digits is extremely useful information. I have read the references and coded the assignments several times never made the connection, and probably never would have made the connection. So much easier.
Thanks again for the info.
A silly question however, I am a newbie to the community, how do I mark it as "best" to close it out?