Skip to main content
STee.3
Associate II
March 22, 2023
Solved

RTC is getting set off by 1hour in STM32U5. I am using Nucleo board and I am checking the RTC behavior in STOP3 mode of stm32u5.

#include "main.h"
#include <stdio.h>
#include <string.h>
RTC_HandleTypeDef hrtc;
 
UART_HandleTypeDef huart1;
 
/* USER CODE BEGIN PV */
#define UartHandle &huart1
#define RtcHandle &hrtc
static uint16_t YearStart = 2000;
 
char message[50];
uint8_t size;
 
uint8_t Rx_data;
 
void SystemClock_Config(void);
static void SystemPower_Config(void);
static void MX_GPIO_Init(void);
static void MX_RTC_Init(void);
static void MX_USART1_UART_Init(void);
 
void set_time (void)
{
	RTC_TimeTypeDef sTime;
	 RTC_DateTypeDef sDate;
 
	 size = sprintf(message, "\n\r RTC in Stop Mode\n\r");
	 HAL_UART_Transmit(UartHandle, (uint8_t*)message, size, 100);
 
	 // Set date and time
	 sDate.WeekDay = RTC_WEEKDAY_TUESDAY;
	 sDate.Date = 22;
	 sDate.Month = 03;
	 sDate.Year = 23; // from 0-99 (1972 == 72, start year = 1900)
	 HAL_RTC_SetDate(RtcHandle, &sDate, RTC_FORMAT_BIN);
	 sTime.Hours = 10;
	 sTime.Minutes = 45;
	 HAL_RTC_SetTime(RtcHandle, &sTime, RTC_FORMAT_BIN);
 
	 HAL_RTCEx_BKUPWrite(RtcHandle, RTC_BKP_DR0, 0xBEBE);
 
}
void get_time(void)
{
 
 static RTC_TimeTypeDef sTime;
		static RTC_DateTypeDef sDate;
		static char message[50];
		static size_t size;
 
		// Get current time and date
 
		HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
		HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
 
		// Send time and date over uart
		size = sprintf(message, "Date: %2.2u-%2.2u-%4.4u Time: %2.2u:%2.2u:%2.2u\n\r", sDate.Date, sDate.Month, sDate.Year + YearStart,sTime.Hours, sTime.Minutes, sTime.Seconds);
		HAL_UART_Transmit(UartHandle, (uint8_t*)message, size, 100);
		HAL_Delay(1000);
 
}
 
void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
	if(GPIO_Pin == GPIO_PIN_13)
	{
		 SystemClock_Config();
 
			size = sprintf(message, "\n\r After Sleep Mode \n\r");
		 HAL_UART_Transmit(UartHandle, (uint8_t*)message, size, 100);
		 get_time();
	}
 
}
 
int main(void)
{
 
 HAL_Init();
 
 SystemClock_Config();
 
 SystemPower_Config();
 
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_RTC_Init();
 MX_USART1_UART_Init();
 /* USER CODE BEGIN 2 */
 if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR0) != 0xBEBE )
 {
 set_time();
 }
 size = sprintf(message, "\n\r Before Stop Mode \n\r");
 HAL_UART_Transmit(UartHandle, (uint8_t*)message, size, 50);
 get_time();
 
 /* Check and Clear the Wakeup flag */
 /* Enable Backup domain access */
 
 
 HAL_SuspendTick();
 
 // wake up using external interrupt using user button
 HAL_PWREx_EnterSTOP3Mode(PWR_STOPENTRY_WFI);
	
 HAL_ResumeTick();
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE4) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
 
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief Power Configuration
 * @retval None
 */
static void SystemPower_Config(void)
{
 
 /*
 * Switch to SMPS regulator instead of LDO
 */
 if (HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY) != HAL_OK)
 {
 Error_Handler();
 }
}
 
static void MX_RTC_Init(void)
{
 
 /* USER CODE BEGIN RTC_Init 0 */
 
 /* USER CODE END RTC_Init 0 */
 
 RTC_PrivilegeStateTypeDef privilegeState = {0};
 
 /* USER CODE BEGIN RTC_Init 1 */
 
 /* USER CODE END RTC_Init 1 */
 
 /** Initialize RTC Only
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = 127;
 hrtc.Init.SynchPrediv = 255;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
 hrtc.Init.BinMode = RTC_BINARY_NONE;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }
 privilegeState.rtcPrivilegeFull = RTC_PRIVILEGE_FULL_NO;
 privilegeState.backupRegisterPrivZone = RTC_PRIVILEGE_BKUP_ZONE_NONE;
 privilegeState.backupRegisterStartZone2 = RTC_BKP_DR0;
 privilegeState.backupRegisterStartZone3 = RTC_BKP_DR0;
 if (HAL_RTCEx_PrivilegeModeSet(&hrtc, &privilegeState) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN RTC_Init 2 */
 
 /* USER CODE END RTC_Init 2 */
 
}
 
}
 
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
 /*Configure GPIO pin : PC13 */
 GPIO_InitStruct.Pin = GPIO_PIN_13;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI13_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI13_IRQn);
 
}

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
March 22, 2023

Initialize the local structs in set_time():

void set_time (void)
{
	RTC_TimeTypeDef sTime = {0};
	 RTC_DateTypeDef sDate = {0};
...

JW

2 replies

LCE
Principal III
March 22, 2023

Exactly 1 hour?

Daylight Saving Time?

waclawek.jan
waclawek.janBest answer
Super User
March 22, 2023

Initialize the local structs in set_time():

void set_time (void)
{
	RTC_TimeTypeDef sTime = {0};
	 RTC_DateTypeDef sDate = {0};
...

JW