Skip to main content
ngodoanvan
Associate III
Jul 20, 2022 2:52 PM UTC
Question

RTC Initialization have a problem.

Hi

I created my new project follow SubGHz Phy Ping Pong example project. This is my MX_RTC_Init() function:

void MX_RTC_Init(void)
{
 
 /* USER CODE BEGIN RTC_Init 0 */
 
 /* USER CODE END RTC_Init 0 */
 
 RTC_TimeTypeDef sTime = {0};
 RTC_DateTypeDef sDate = {0};
 RTC_AlarmTypeDef sAlarm = {0};
 
 /* USER CODE BEGIN RTC_Init 1 */
 
 /* USER CODE END RTC_Init 1 */
 
 /** Initialize RTC Only
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = RTC_PREDIV_A;
 hrtc.Init.SynchPrediv = RTC_PREDIV_S;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
 hrtc.Init.BinMode = RTC_BINARY_NONE;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* USER CODE BEGIN Check_RTC_BKUP */
	if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR10) != 0x32F2)
	{
 /* USER CODE END Check_RTC_BKUP */
 
 /** Initialize RTC and set the Time and Date
 */
 sTime.Hours = 0x0;
 sTime.Minutes = 0x0;
 sTime.Seconds = 0x0;
 sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
 sTime.StoreOperation = RTC_STOREOPERATION_RESET;
 if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
 {
 Error_Handler();
 }
 sDate.WeekDay = RTC_WEEKDAY_MONDAY;
 sDate.Month = RTC_MONTH_JANUARY;
 sDate.Date = 0x1;
 sDate.Year = 0x0;
 if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Enable the Alarm A
 */
 sAlarm.AlarmTime.Hours = 0x0;
 sAlarm.AlarmTime.Minutes = 0x0;
 sAlarm.AlarmTime.Seconds = 0x0;
 sAlarm.AlarmTime.SubSeconds = 0x0;
 sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
 sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;
 sAlarm.AlarmMask = RTC_ALARMMASK_NONE;
 sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_NONE;
 sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
 sAlarm.AlarmDateWeekDay = 0x1;
 sAlarm.Alarm = RTC_ALARM_A;
 if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Enable the Alarm B
 */
 sAlarm.AlarmTime.Seconds = 0x10;
 sAlarm.AlarmMask = RTC_ALARMMASK_DATEWEEKDAY|RTC_ALARMMASK_HOURS
 |RTC_ALARMMASK_MINUTES;
 sAlarm.Alarm = RTC_ALARM_B;
 if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Enable the WakeUp
 */
 if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 0) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN RTC_Init 2 */
	HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKP_DR10, 0x32F2);
	}
 /* USER CODE END RTC_Init 2 */
 
}

First time, I write 0x32F2 to BackUp register 10. The TIMER_IF_Init() function below,

UTIL_TIMER_Status_t TIMER_IF_Init(void)
{
 UTIL_TIMER_Status_t ret = UTIL_TIMER_OK;
 /* USER CODE BEGIN TIMER_IF_Init */
 
 /* USER CODE END TIMER_IF_Init */
 if (RTC_Initialized == false)
 {
 hrtc.IsEnabled.RtcFeatures = UINT32_MAX;
 /*Init RTC*/
 MX_RTC_Init();
 /*Stop Timer */
 TIMER_IF_StopTimer();
 /** DeActivate the Alarm A enabled by STM32CubeMX during MX_RTC_Init() */
 HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A);
 /*overload RTC feature enable*/
 hrtc.IsEnabled.RtcFeatures = UINT32_MAX;
 
 /*Enable Direct Read of the calendar registers (not through Shadow) */
 HAL_RTCEx_EnableBypassShadow(&hrtc);
 /*Initialize MSB ticks*/
 TIMER_IF_BkUp_Write_MSBticks(0);
 
 TIMER_IF_SetTimerContext();
 
 /* Register a task to associate to UTIL_TIMER_Irq() interrupt */
 UTIL_TIMER_IRQ_MAP_INIT();
 
 RTC_Initialized = true;
 }
 
 /* USER CODE BEGIN TIMER_IF_Init_Last */
 
 /* USER CODE END TIMER_IF_Init_Last */
 return ret;
}

My project run without no stuck in first time. When I reset MCU, my project stuck when called PWR_ExitStopMode().

What wrong in my code.

Anyone know how to fix this problem? Please support me.

This topic has been closed for replies.