RTC can't work because PLL already use
Dear Sir:
I had reference the PWR_STANDBY_RTC sample code form STM32Cube_FW_L4_V1.8.0
This sample code are work well and wake up about 30 second,
but after move to my code get return fail at
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) form
SystemClock_Config()void SystemClock_Config(void)
{......
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLP = 7; RCC_OscInitStruct.PLL.PLLQ = 4; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {// return here.while(1);
}after check, find is because PLL already used?
/* Check if the PLL is used as system clock or not */
if(__HAL_RCC_GET_SYSCLK_SOURCE() != RCC_CFGR_SWS_PLL) {.......
else
{ return HAL_ERROR; }I have reference this web say need turn off some content of
SystemInit()
https://www.mianbaoban.cn/blog/post/45024
but still don't work, then how to use PLL and let SystemClock_Config?
Thx for your answer.