Skip to main content
acer
Associate
Sep 6, 2013 12:32 PM UTC
Question

RTC Calibration STM32F205

Posted on September 06, 2013 at 14:32

I'm trying to calibrate the difference of 512Hz at the out  where PC13 possess 511.936Hz which causes about 10 seconds per day delay in the RTC. I'm making the form below, I wonder where I'm going wrong, not because it was effective, I do not find application notes with the correct sequence programming

//   ((511.936-511.968)/511.9868) x 1 E06 =   -62,5

//   Looking in calibration table, the nearest compensation value is 65

//  And then: 

status_error = RTC_CoarseCalibConfig(RTC_CalibSign_Positive, 65);

status_error = RTC_CoarseCalibCmd(ENABLE); 

Does not effect !!!!!!! Somebody help me

#calibration-rtc-stm32-f205
This topic has been closed for replies.