Skip to main content
Associate
May 5, 2025
Question

RTC Calibration

  • May 5, 2025
  • 3 replies
  • 497 views

I have selected the RTC calibration as 512Hz. Will I be able to perform RTC smooth calibration if my frequency obtained on the RTC calib pin is beyond the range 511.75Hz - 512.25Hz. 

How do I calibrate the RTC beyond this range ?? 

 

This topic has been closed for replies.

3 replies

TDK
May 5, 2025

From the reference manual:

The RTC frequency can be digitally calibrated with a resolution of about 0.954 ppm with a
range from -487.1 ppm to +488.5 ppm.

If your crystal is outside of those limits, you will be unable to calibrate it with this method. Since crystals are typically accurate to well under 100 ppm, there is plenty of margin.

 

If your clock is outside of that range, choosing a more accurate clock source is probably the best option.

"If you feel a post has answered your question, please click ""Accept as Solution""."
J_ThomasAuthor
Associate
May 7, 2025

Thank you so much!

mbarg.1
Senior III
May 6, 2025

Double check which oscillator you are using for RTC - some time it uses as default internal RC instead of external crystal.