Skip to main content
nicolas
Senior II
Nov 18, 2025 12:37 PM UTC
Solved

RTC: are interrupt flag set during Vbat mode

I have a STM32U595 and I use the RTC in binary mode.

If an SSR underflow occurs during Vbat mode, will the SSRUF be set so after power recovery I can manage the interrupt ?

ELABI.1
ELABI.1Best answer
ST Technical Moderator
Nov 20, 2025 1:32 PM UTC

Hi @nicolas,

Yes, SSRUF will still be set when VDD is back, with interrupt generation, which can then be served after NVIC initialization.

You can refer to the Reference Manual RM0456 section 63 Real-time clock (RTC) for more information.

Thanks.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

ELABI.1
ELABI.1Best answer
ST Technical Moderator
Nov 20, 2025 1:32 PM UTC

Hi @nicolas,

Yes, SSRUF will still be set when VDD is back, with interrupt generation, which can then be served after NVIC initialization.

You can refer to the Reference Manual RM0456 section 63 Real-time clock (RTC) for more information.

Thanks.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
nicolas
nicolasAuthor
Senior II
Nov 20, 2025 2:03 PM UTC

Thank you for the answer. I did look on the RM0456 but I didn't found this information.