Skip to main content
Associate
September 19, 2024
Solved

RMII diagrams

Hi, we are working with a STM32F217 and the RMII bus.

In the two documents reported I see an inconsistency on the diagrams (on the one hand rising edge sampling, on the other falling edge). Which one is correct for my chip?

RM0033 Figure 328 Reference Manual (01 Mar 2021) 

DS6697 Figure 48Product Specification (05 Sep 2016) 

 

BR

Stefano

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
September 23, 2024

Hi @StefanoRossi ,

The RMII operates using the rising edge of the clock signal for both TX and RX data transfers.

So, the DS6697 Rev 13 - Figure 48. Ethernet RMII timing diagram is the correct one.

This RM0033 will be updated to fix the issue.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

ST Technical Moderator
September 19, 2024

Hello @StefanoRossi and welcome to ST Community,

Thank you for having reported the point.

I escalated this request to involved people for review and take the necessary action.

(Internal ticket number: 191487 - this ticket number is only for reference, not available outside of ST)

I'll make sure to post updates here as soon as possible. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
September 23, 2024

Hi @StefanoRossi ,

The RMII operates using the rising edge of the clock signal for both TX and RX data transfers.

So, the DS6697 Rev 13 - Figure 48. Ethernet RMII timing diagram is the correct one.

This RM0033 will be updated to fix the issue.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks