Skip to main content
Associate II
Oct 23, 2026 8:46 AM UTC
Question

RM0468 Figure 297. Comparator functional block diagram error.

Hi everyone,

While using the comparator interrupt functionality, I discovered an error in the comparator block diagram provided in the Reference Manual for the H723 series(RM0468):

As shown in the image above, the signal that triggers the interrupt does not actually pass through the polarity selection stage; instead, it is routed to the interrupt logic immediately after the comparator output. My evidence is as follows:
First, I observed that a specific output state causes the interrupt to trigger continuously (making it impossible to clear the `CC1IF` flag). Upon checking the block diagram, I saw that `CC1IF = cmp1_out & ITEN`, which implies that setting `cmp1_out` to 0 should resolve the issue. However, in practice, this has no effect—the `CC1IF` flag remains set. The only way to clear `CC1IF` is to adjust the comparator inputs to invert the comparator's output.
These are the results I obtained from testing on an STM32H723ZGT6.

3 replies

KDJEM.1
ST Technical Moderator
Oct 26, 2026 2:46 PM UTC

Hello ​@Philister ,

 

Are you talking about this figure? 

What changes do you propose based on tests?

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
PhilisterAuthor
Associate II
Oct 28, 2026 3:33 AM UTC

Hi ​@KDJEM.1 

Yes, apologies—I failed to upload the image. What I meant to convey is that the actual behavior of the chip is as follows:

This global interrupt signal does not undergo any polarity selection.

 

Best Regards,

Daniel.

KDJEM.1
ST Technical Moderator
Nov 2, 2026 10:04 AM UTC

Hello ​@Philister  ;

 

To reproduce the issue, could you please share the test project?

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.