Skip to main content
Visitor
Jun 30, 2026 1:13 PM UTC
Solved

RM0468 - BOR_LVL discrepancy

Hi

While reviewing some specs for the SW developers, we noticed some inconsitency between the datasheet and reference manual of the STM32H735.

The DS states four VBOR thresholds (VBOR0 to VBOR3).

In the RM, the description of Bits 3:2 BOR_LEV[1:0] is different for the read-only register FLASH_OPTSR_CUR and the programming register FLASH_OPTSR_PRG. The former states four VBOR thresholds (VBOR2 is 0b10), the latter refers to a nominal voltage level (2.4V - approx. VBOR2 - is 0b01). 

Can you please clarify. 

Thanks! 

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Jun 30, 2026 2:03 PM UTC

Hello ​@embd and welcome to the community;

 

Thank you for reporting this issue.

 The BOR_LEV bit description in FLASH_OPTSR_PRG  should be:
Bits 3:2 BOR_LEV: Brownout level option configuration bit
These option bits are used to define the power level that generates a system reset.
00: VBOR0, brownout reset threshold 0
01: VBOR1, brownout reset threshold 1
10: VBOR2, brownout reset threshold 2
11: VBOR3, brownout reset threshold 3

This issue is already reported internally for checking and fixing.

Internal ticket number 139749 (This is an internal tracking number and is not accessible or usable by customers).  

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

1 reply

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Jun 30, 2026 2:03 PM UTC

Hello ​@embd and welcome to the community;

 

Thank you for reporting this issue.

 The BOR_LEV bit description in FLASH_OPTSR_PRG  should be:
Bits 3:2 BOR_LEV: Brownout level option configuration bit
These option bits are used to define the power level that generates a system reset.
00: VBOR0, brownout reset threshold 0
01: VBOR1, brownout reset threshold 1
10: VBOR2, brownout reset threshold 2
11: VBOR3, brownout reset threshold 3

This issue is already reported internally for checking and fixing.

Internal ticket number 139749 (This is an internal tracking number and is not accessible or usable by customers).  

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.