Skip to main content
Uwe Bonnes
Chief
January 29, 2026
Solved

RM0456: 33.4.8 Extended calibration mode: Missing reset of ADC_CR_ADCALLIN bit?

Hello,

ADC_CR_ADCALLIN is described as "rw" . The procedure given in RM0456: 33.4.8 Extended calibration mode does not explicit recommend to reset ADC_CR_ADCALLIN after the procedure. I think it is helpfull to add in RM0456.

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
January 30, 2026

Hi @Uwe Bonnes ,

I got this internal feedback:

"One could clear the bit, but only if one wants to switch off the linearity calibration for another calibration. In typical use, there would be only need to calibrate once. When the calibration is lost, for example in reset, the bit is also reset. Leaving the bit set is probably closer to typical usage. There's usually no point in clearing it by SW."

Hope it does answer your question

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

mƎALLEm
ST Technical Moderator
January 29, 2026

Hello,

I will check internally and get back to you with a feedback. Internal ticket number for follow-up: 226212.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
January 30, 2026

Hi @Uwe Bonnes ,

I got this internal feedback:

"One could clear the bit, but only if one wants to switch off the linearity calibration for another calibration. In typical use, there would be only need to calibrate once. When the calibration is lost, for example in reset, the bit is also reset. Leaving the bit set is probably closer to typical usage. There's usually no point in clearing it by SW."

Hope it does answer your question

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.