Skip to main content
Andreas Bolsch
Lead III
Jun 7, 2021 7:47 PM UTC
Solved

RM0455: STM32H7A/B Reset value of PWR_SRDCR incorrect

Rev. 5 of RM0455 says "Reset value: 0x0000 4000" for PWR_SRDCR.

However, the description "Bits 15:14 VOS[1:0]: 00: scale 3 (default)" contradicts this. And on actual hardware reset value is indeed 0x00002000.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jun 8, 2021 2:08 PM UTC

Hi @Andreas Bolsch​ ,

You are right, even the Rev 6 is wrong an the Reset value should be 0x00002000 (not 0x0000 4000).

This will be corrected in the coming reference manual revisions.

Thanks for your contribution.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

ST Technical Moderator
Jun 8, 2021 8:01 AM UTC

Hello @Andreas Bolsch​ ,

Thanks you for noticing us.

I will check this and raise it internally to take the necessary action.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
Jun 8, 2021 2:08 PM UTC

Hi @Andreas Bolsch​ ,

You are right, even the Rev 6 is wrong an the Reset value should be 0x00002000 (not 0x0000 4000).

This will be corrected in the coming reference manual revisions.

Thanks for your contribution.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks