Skip to main content
Andreas Bolsch
Lead III
Jun 17, 2021 4:26 PM UTC
Solved

RM0455 STM32H7A/B: Reset state of SYSCFG_PMCR incorrect?

RM0455, rev. 6, says reset state of SYSCFG_PMCR is 0x0F00 0000.

But STM32H7A3ZIT6Q, rev. Z, shows 0x0300 0000 instead, i.e. PC2 and PC3 switches closed. not open. Does this depend on package as PC2 and PC3 are not bonded out for this particular package?

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jun 18, 2021 7:48 AM UTC

Hello @Andreas Bolsch (Community Member)​ ,

In fact, the value depends on the packages.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

8 replies

TDK
Jun 17, 2021 8:59 PM UTC

FWIW, on my STM32H7B3I-DK board, the reset value is 0, barring any bugs in the SVD file. That chip has all 8 pins present.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andreas Bolsch
Lead III
Jun 18, 2021 5:38 AM UTC

Hm, for STM32H7B3LIH6Q, rev. Z, on STM32H7B3I-DK I see reset value 0x0F00 0000 ...

That you observed 0 might be due to disabled clock, i.e. SYSCFGEN in RCC_APB4ENR not being set.

Imen.DBest answer
ST Technical Moderator
Jun 18, 2021 7:48 AM UTC

Hello @Andreas Bolsch (Community Member)​ ,

In fact, the value depends on the packages.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
waclawek.jan
Super User
Jun 18, 2021 7:58 PM UTC

Shouldn't that still be properly documented?

JW

ST Technical Moderator
Jul 1, 2021 9:48 AM UTC

Hi @Community member​ ,

I raised the same feedback internally :)

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
waclawek.jan
Super User
Jul 1, 2021 10:56 AM UTC

Thanks, Imen.

Jan