Skip to main content
Singh.Harjit
Senior
Oct 5, 2020 5:38 AM UTC
Solved

RM0440, Rev 4, STM32G4 Reference Manual - typos

Table 226 on page 906 has an entry HRTIM_TIMxCMP1CR <- I don't think this is a real register.

Section 27.3.8, page 888 second line in last paragraph says "any of the 5 timers". I think that should be 6 timers.

Section 27.5.66, page 1050 says Bits 31:0 Refer to HRTIM_ADC1R bits description <- this should be HRTIM_ADC3R

Section 27.5.67, page 1051 says Bits 31:0 Refer to HRTIM_ADC2R bits description <- this should be HRTIM_ADC4R

Section 27.5.69, page 1055 has a footnote that should be at the end of section 27.5.68, page 1053.

Section 27.5.68, page 1052 bit descriptions call out "ADC trigger 3 ...". If this same description is used for HRTIM_ADC1R, then the trigger number is wrong i.e. it should be "ADC trigger 1 ...".

Section 27.5.69, page 1054 bit descriptions call out "ADC trigger 4 ...". If this same description is used for HRTIM_ADC2R, then the trigger number is wrong i.e. it should be "ADC trigger 2 ...".

This topic has been closed for replies.
Imen GH
Imen GHBest answer
ST Employee
Oct 5, 2020 9:33 AM UTC

Hello

Thanks for your contribution.

I will raise your reported case internally to take into consideration.

Imen

1 reply

Imen GH
Imen GHBest answer
ST Employee
Oct 5, 2020 9:33 AM UTC

Hello

Thanks for your contribution.

I will raise your reported case internally to take into consideration.

Imen