Skip to main content
Uwe Bonnes
Chief
July 26, 2018
Question

RM0433, DMA/BDMA: Wrong memory region as source/target will set FIFO error!

  • July 26, 2018
  • 2 replies
  • 679 views

While bringing up DMA on H743 in my code, I painfully found out that specifying a wrong memory region as DMA target, like ITCM for DMA transfers, will also set a FIFO error and abort transmission. RM0433 should mention wrong SRAM source or target regions as possible cause for a FIFO error.

Please clarify the reference manual.

This topic has been closed for replies.

2 replies

Amel NASRI
ST Technical Moderator
August 1, 2018

Hi @Uwe Bonnes​ ,

There is no FIFO for BDMA.

However, to get more details about FIFO when using DMA, please refer to AN4031 (https://www.st.com/content/ccc/resource/technical/document/application_note/27/46/7c/ea/2d/91/40/a9/DM00046011.pdf/files/DM00046011.pdf/jcr:content/translations/en.DM00046011.pdf).

That is true STM32H7 isn't yet supported in the application note, but almost the same behavior is described there.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Uwe Bonnes
Chief
August 2, 2018

I think your answer did not get the point of my question. The question was not about FIFO mode. Even in direct mode, H743 DMA will flag a FIFO error when a wrong memory region is specified as target for the DMA. "RM0433 should mention wrong SRAM source or target regions as possible cause for a FIFO error."