Skip to main content
SSorr.1
Associate II
March 22, 2021
Solved

Revert .ioc file for older CubeIde version

  • March 22, 2021
  • 4 replies
  • 4793 views

Hello,

I recently upgraded to CubeIde 1.6.0 but I am having many new problems when programming STM32h/43: the configurations generation is much slower and it often stops updating all needed files, which forces me to reboot (I could not find a better way).

So I decided to downgrade to 1.5.1 which was stable for me, but I cannot load the .ioc files that were generated with 1.6.0. Is there a workaround?

This topic has been closed for replies.
Best answer by CCend.2

Open the IOC file in a text editor and change the line "MxCube.Version=***" to the version of CubeMX that your version of the IDE wants you to have.

4 replies

Tesla DeLorean
Guru
March 22, 2021

>>Is there a workaround?

I'm sensing there isn't, I guess you could try a text editor or a merge tool to understand the change in features/structure.

Importing older .IOC has been a challenge at times, I'd definitely recommend doing this into a sandbox project rather than a live one, as file loss has been reported on multiple occasions.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
CCend.2
CCend.2Best answer
Associate II
May 4, 2023

Open the IOC file in a text editor and change the line "MxCube.Version=***" to the version of CubeMX that your version of the IDE wants you to have.

Explorer
October 10, 2023

wow, it really works for opening the 6.3.0 version ioc file by cubemx 6.2.0, thanks bro