Skip to main content
marcus2399
Associate II
August 17, 2009
Question

Returning from nested exceptions.

  • August 17, 2009
  • 4 replies
  • 927 views
Posted on August 17, 2009 at 18:34

Returning from nested exceptions.

    This topic has been closed for replies.

    4 replies

    marcus2399
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:20

    Hi!

    I just ran into a small problem - at the end of an exception handler, I have to decide whether to return using the process stack or the main stack. I also need to select handler mode or thread mode. So far, in my kernel, I only have an SVC handler, so I will always return to thread mode and process stack.

    However when supporting nested interrupts I need to keep track myself if there are any lower-priority exceptions pending to know how to return. So I need to maintain a counter of nested exceptions.

    Is this the way it should be or have I misunderstood something?

    Best Regards and TIA,

    Marcus

    guyvo67
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:20

    Some good example on SVC, PENDV and working with EXEC return values can be found in the freeRTOS port for the cortex. More particular in the file port.c

    http://www.freertos.org/

    Perhaps you can take look into to brighten you idea's.

    Guy

    picguy
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:20

    The common simple case is simple. All exceptions and interrupts return to whatever was interrupted. A normal bx lr or C/C++ subroutine return always works. No special s/w games are required. Nested interrupts et al work just fine.

    However, if you need to return elsewhere you need to set SP such that r0-r3 & r12, lr, pc & xPSW are restored. Set r5-11 if needed. Then set lr=FFFFFF?? then bx lr. Set ?? for the stack and protection mode you need. (You may set any r0-r12 to the magic value and bx the magic value register.)

    marcus2399
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:20

    Apparently, I did not read the Exception Return chapter of the Architecture Reference Manual carefully enough; back to school! ;) Thanks to both of you. I'll also take a look at the FreeRTOS port.

    EDIT: I see now how the LR register is set properly by the PushStack operation during the exception extry. From there it is clear that a bx lr will cut it!

    [ This message was edited by: marcus.johansson on 17-08-2009 22:08 ]