Question
RESOLVED: TIM3 - 50 Hz pulse
Posted on October 13, 2016 at 00:41
Hello,
Will the following generate a 50 Hz pulse?(Since htim3.Init.Period = 19999 which I think equates to ~20ms) htim3.Instance = TIM3; htim3.Init.Prescaler = 83; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 19999; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; if (HAL_TIM_Base_Init(&htim3) != HAL_OK) { Error_Handler(); }Thanks,Sel