Skip to main content
infoinfo966
Associate II
July 22, 2011
Question

Resetting a Timer

  • July 22, 2011
  • 2 replies
  • 744 views
Posted on July 22, 2011 at 09:04

Hi,

I have the following problem.

I have a RFID-Reader Chips from Melexis (90109) connected to two GPIO Pins (Clock and Data).

I process the incoming data with an EXTI handler that is triggert on the falling edge of the clock pin.

This works fine.

To detect if a transponder has left the field I must detect if the clock line is no longer atcive for a certain amount of time.

My current approach is that I set up TIM2 as normal Timebase counter with an TIM_UPDATE IRQ-Handler as sort of watch dog for the clock line.

In the EXTI handler I tried to reset TIM2 with

  TIM_SetCounter(TIM2, 0);

so that as long as I receive clock pulses shorter than the timer period, the TIM2 Handler should not be called at all.

If the clock stops, TIM2 handler should set a flag to signals the main loop that the transponder was removed.

So far the idea, but reality shows that although I reset the TIM2 counter regulary I always get the TIM2 IRQ in it's normal period.

Do I have to reset/restart a timer in a different way?

Best

Tom
    This topic has been closed for replies.

    2 replies

    greg_t
    Associate III
    July 23, 2011
    Posted on July 23, 2011 at 20:29

    Hello,

    Please post your TIM2 configuration

    infoinfo966
    Associate II
    July 25, 2011
    Posted on July 25, 2011 at 11:03

    Hi,

    here is my TIM2 config

    // Timer to detect if transponder was removed

    #define

    TIMER_TAKT

    10000

    /* Timer wird mit 10kHz getaktet */

    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

    uint16_t PrescalerValue;

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

    // TIMER 2 Takt freigeben

    PrescalerValue = (uint16_t) (SystemCoreClock / TIMER_TAKT) -

    1

    ;

    // Vorteiler berechnen

    // Timer Grundkonfiguration

    TIM_TimeBaseStructure.TIM_Period =

    100

    ;

    // Timer zählt von 0 ... 100: also alle 10ms

    TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;

    TIM_TimeBaseStructure.TIM_ClockDivision =

    0

    ;

    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

    TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

    // Timer einstellen

    //Timer Vorteiler-Taktkonfiguration

    TIM_PrescalerConfig(TIM2, PrescalerValue, TIM_PSCReloadMode_Immediate);

    // Auto-Reload

    // Timer aktivieren

    TIM_Cmd(TIM2, ENABLE);

    NVIC_InitTypeDef NVIC_InitStructure;

    /* Enable the Interrupt */

    NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority =

    0

    ;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority =

    1

    ;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);

    I attach an Screenshot of my LA, where you can see the clock in wich EXTI do

    TIM_SetCounter(TIM2,

    0

    );

    // reset watchdog counter as we still receive clock ticks

    In the timer IRQ handler I toggle an IO port, which you can see in the bottom line:

    Best

    Tom

    ________________

    Attachments :

    Timer-Reset.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0rh&d=%2Fa%2F0X0000000bh5%2FPh6rP86fHT35bOaqG049yYz0VZ45GVztBJnFD5uCOfc&asPdf=false