Skip to main content
daneichenwald1
Associate
April 17, 2009
Question

Reseting the STLM75 Temperature sensor

  • April 17, 2009
  • 2 replies
  • 721 views
Posted on April 17, 2009 at 15:23

Reseting the STLM75 Temperature sensor

    This topic has been closed for replies.

    2 replies

    nanayakkaraan
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:10

    Hello Dan,

    I am also facing the same problem you did, in I2C communication with STLM75 temperature sensor.

    ''Write Addr -> Always generates Acknowledge Failure Error ''

    I have been receiving this error and trying to figure out how to overcome it.

    Have you found any solutions?

    Any advice on this matter is appreciated.

    Thank you.

    daneichenwald1
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:10

    I have my I2C drivers working as I can read and write to I2C devices. I'm working with the STLM75 Temperature sensor on the eval board. However, I noticed that if an I2C transfer gets interrupted, I can no longer talk to that device. The simplest case is:

    1. Generate a START

    2. Reset the processor

    3. Generate a START

    4. Write Addr -> Always generates Acknowledge Failure Error

    5. Reset the processor

    6. Works fine

    I've tried generating various combinations of START/STOPs on every reset, but I can't seem to reset the temp sensor. (if that is even the problem) My code is basically taken directly from STM eval example.

    Thanks in advance!

    Dan