reset on nucleo -f401RE with even very simple main loop
Dear Sir/Madam:
I am using nucleo -f401RE with STM32 . I found the program keeps reset even with almost empty main loop
there is no way to do seftreset from the codes.
only settings for hardware are system clock and some hall_init
any clue why it is reset?
here are the ref code:
int main(void)
{
//=================================================================
// Initialize everything /* STM32F4xx HAL library initialization: - Configure the Flash prefetch, instruction and Data caches - Configure the Systick to generate an interrupt each 1 msec - Set NVIC Group Priority to 4 - Global MSP (MCU Support Package) initialization */ HAL_Init(); // My local init Init();static bool fcFlag = false;
// Set up variables related to state machineint main_state = START; //================================================================= // Now loop forever and cycle through states while(1) { switch (main_state) { case START: if ( fcFlag == false ) { STROBE(START) // send to gp PC8 pin to scope to check reset fcFlag = true; }break;
default:
}// switch
//===============================================
int Init(void) {
GPIO_InitTypeDef GPIO_InitStruct; /*######## Configure the system clock to 84 MHz ############################*/ SystemClock_Config();/*######## Turn on GPIO clocks ############################*/
__GPIOA_CLK_ENABLE(); __GPIOB_CLK_ENABLE(); __GPIOC_CLK_ENABLE(); // Now turn on pin PC8 used for debug. GPIO_InitStruct.Pin = GPIO_PIN_8; GPIO_InitStruct.Speed = GPIO_SPEED_MEDIUM; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);return 0;
} // end of Init
//=======================================
//===============================================================================
// Private fcns./*-------------------------------------------------------------*/
/*** @brief System Clock Configuration* The system Clock is configured as follow : * System Clock source = PLL (HSI)* SYSCLK(Hz) = 84000000* HCLK(Hz) = 84000000* AHB Prescaler = 1* APB1 Prescaler = 2* APB2 Prescaler = 1* HSI Frequency(Hz) = 16000000* PLL_M = 16* PLL_N = 336* PLL_P = 4* PLL_Q = 7* VDD(V) = 3.3* Main regulator output voltage = Scale2 mode* Flash Latency(WS) = 2* @param None* @retval None*/static void SystemClock_Config(void){ RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_OscInitTypeDef RCC_OscInitStruct; /* Enable Power Control clock */ __HAL_RCC_PWR_CLK_ENABLE(); /* The voltage scaling allows optimizing the power consumption when the device is clocked below the maximum system frequency, to update the voltage scaling value regarding system frequency refer to product datasheet. */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2); /* Enable HSI Oscillator and activate PLL with HSI as source */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 0x10; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 16; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4; RCC_OscInitStruct.PLL.PLLQ = 7; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */ RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); }}//============================================================
/**
* @brief This function is used to initialize the HAL Library; it must be the first * instruction to be executed in the main program (before to call any other * HAL function), it performs the following: * Configure the Flash prefetch, instruction and Data caches. * Configures the SysTick to generate an interrupt each 1 millisecond, * which is clocked by the HSI (at this stage, the clock is not yet * configured and thus the system is running from the internal HSI at 16 MHz). * Set NVIC Group Priority to 4. * Calls the HAL_MspInit() callback function defined in user file * 'stm32f4xx_hal_msp.c' to do the global low level hardware initialization * * @note SysTick is used as time base for the HAL_Delay() function, the application * need to ensure that the SysTick time base is always set to 1 millisecond * to have correct HAL operation. * @retval HAL status */HAL_StatusTypeDef HAL_Init(void){ /* Configure Flash prefetch, Instruction cache, Data cache */ #if (INSTRUCTION_CACHE_ENABLE != 0U) __HAL_FLASH_INSTRUCTION_CACHE_ENABLE();#endif /* INSTRUCTION_CACHE_ENABLE */#if (DATA_CACHE_ENABLE != 0U)
__HAL_FLASH_DATA_CACHE_ENABLE();#endif /* DATA_CACHE_ENABLE */#if (PREFETCH_ENABLE != 0U)
__HAL_FLASH_PREFETCH_BUFFER_ENABLE();#endif /* PREFETCH_ENABLE *//* Set Interrupt Group Priority */
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);/* Use systick as time base source and configure 1ms tick (default clock after Reset is HSI) */
HAL_InitTick(TICK_INT_PRIORITY); /* Init the low level hardware */ HAL_MspInit(); /* Return function status */ return HAL_OK;}