Skip to main content
John Doe1
Associate III
Jan 20, 2019 3:50 PM UTC
Solved

reset all MAC subsystem internal registers and logic - fail?

DMABR->SR should be auto-cleared when set 1.

I haven't modified code - auto generated by hal.

It always timeouts - any ideas why? I tried to extend timeout time - bit 0 is always 1.

Here is code from HAL:

 /* Ethernet Software reset */
 /* Set the SWR bit: resets all MAC subsystem internal registers and logic */
 /* After reset all the registers holds their respective reset values */
 (heth->Instance)->DMABMR |= ETH_DMABMR_SR;
 
 /* Get tick */
 tickstart = HAL_GetTick();
 
 /* Wait for software reset */
 while (((heth->Instance)->DMABMR & ETH_DMABMR_SR) != (uint32_t)RESET)
 {
 /* Check for the Timeout */
 if((HAL_GetTick() - tickstart ) > ETH_TIMEOUT_SWRESET)
 { 
 heth->State= HAL_ETH_STATE_TIMEOUT;
 
 /* Process Unlocked */
 __HAL_UNLOCK(heth);
 
 /* Note: The SWR is not performed if the ETH_RX_CLK or the ETH_TX_CLK are 
 not available, please check your external PHY or the IO configuration */
 
 return HAL_TIMEOUT;
 }
 }

Bit 0 SR: Software reset When this bit is set, the MAC DMA controller resets all MAC Subsystem internal registers and logic. It is cleared automatically after the reset operation has completed in all of the core clock domains. Read a 0 value in this bit before re-programming any register of the core.

This topic has been closed for replies.
John Doe1
John Doe1Best answer
Associate III
Jan 20, 2019 6:21 PM UTC

Problem solved. I was writing other data to the wrong register.

3 replies

Piranha
Principal III
Jan 20, 2019 5:44 PM UTC

Look for MII/RMII, MAC clocks and pin configuration issues. ETH MAC has 3 main clocks which normally must be enabled and one optional for PTP.

John Doe1
John Doe1Author
Associate III
Jan 20, 2019 5:49 PM UTC

That's really strange. I've been working all day on this mcu and now I'm getting dma error. Didn't make any changes on rmii/mac clocks etc.

John Doe1
John Doe1AuthorBest answer
Associate III
Jan 20, 2019 6:21 PM UTC

Problem solved. I was writing other data to the wrong register.