Skip to main content
Explorer
Nov 2, 2026 10:42 AM UTC
Question

Request for Current Consumption Details – STM32N657X0H3Q (VLXSMPS & VDDCORE Pins)

Hello Everyone,

We are planning to use the STM32N657X0H3Q controller in our upcoming project.

We need to determine the appropriate PCB track widths for the power supply connections. However, the datasheet does not clearly specify the current consumption or current requirements for the VLXSMPS and VDDCORE pins.

Could you please provide the current consumption details for these pins or share any relevant technical documentation or application notes?

This information will help us calculate the required PCB track widths and finalize the power supply layout.

Thank you for your support.

2 replies

EXUE.2
ST Employee
Nov 3, 2026 6:57 AM UTC

Hi, I have no data for your VLXSMPS and VDDCORE pins, but I think you can refer our NUN657X0Q MB1940 board current consumption result. set MCU sysclk=800MHz, RUN: 105mA, SLEEP:94.6mA, STOP:66mA, STANDBY:22.43mA.

jiangfan
ST Employee
Nov 5, 2026 5:34 AM UTC

STM32N6570-DK and NUCLEO-N657X0-Q are ST official boards, you may take them as reference (PCB layout, components)
 

For the STM32N657, VLXSMPS and VDDCORE are part of the internal SMPS power circuit; they are not ordinary external supply pins. There is not one fixed current value for either pin that can be used directly to choose a PCB trace width. Core current depends on the device’s operating conditions and workload.

  • VLXSMPS is the SMPS switching node. Connect it to the inductor as shown in the STM32N657 datasheet’s recommended power-supply schematic. It carries a pulsed switching current, so keep this connection short and use a compact layout; do not route it as a general-purpose power rail.
  • VDDCORE is the core-voltage rail supplied by the SMPS. Connect and decouple it as shown in the datasheet. It is intended for the MCU’s core supply, not as a rail for external loads.

For the layout, follow the datasheet’s SMPS schematic and component/layout guidance, including the specified inductor and capacitors. Size the relevant copper for the expected current, copper thickness, and allowable temperature rise, while keeping the SMPS switching loop compact. Use the datasheet’s power-consumption specifications under your intended voltage, clock, and operating conditions to estimate the overall power demand; the SMPS inductor’s peak and RMS current requirements should be checked against the specified power circuit and component requirements—not inferred from the pin names alone.

The relevant references are the latest STM32N657 datasheet, particularly its power-supply scheme, SMPS application circuit, and electrical-characteristics sections, plus the STM32N6 hardware-design guidance and reference-board schematic/layout.

NOTE: reviewed answer with help of AI