Skip to main content
Chaitanya1
Associate II
April 5, 2023
Question

Replacement for SAF-XC164CS-16F40F BB controller

  • April 5, 2023
  • 4 replies
  • 1334 views

We are looking for a replacement of Infenion microcontroller SAF-XC164CS-16F40F BB. Can you please suggest a suitable ST Microcontroller?

    This topic has been closed for replies.

    4 replies

    Peter BENSCH
    ST Technical Moderator
    April 5, 2023

    Since there is usually no pin-compatible replacement for MCUs, certainly not with 5V supply voltage, you have to pick the appropriate type from the thousands of STM32 derivatives according to your requirements. The product selector available online, for example, helps with this, where you can filter according to your parameters.

    Hope that helps?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Chaitanya1
    Associate II
    April 18, 2023

    Do you have some part numbers that you can suggest as a replacement to SAF-XC164CS-16F40F BB controller? We will modify the controller power & wherever applicable to +3.3V from +5V

    Peter BENSCH
    ST Technical Moderator
    April 18, 2023

    As already mentioned, you can select the appropriate derivative online using the URL above, as no one here knows which parameters of the XC164 are essential for your application. For example, if you need the two CAN modules, you could consider e.g.:

    There are also derivatives with CAN-FD like e.g.:

    And this list is far from complete, so you can see that more requirements are needed to narrow it down. But you can set them as filter parameters online, as mentioned, so that you can narrow down the list quite quickly.

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Good luck!

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Tesla DeLorean
    Guru
    April 5, 2023

    Renesas has a 5V ARM Cortex chip, ST missing an opportunity.​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..