Skip to main content
DSmit.111
Associate
Jul 27, 2021 3:32 PM UTC
Solved

Replace stm32f427vit6 with stm32f427zit6

Hi

can i, if i change the lay-out of my board, replace the original stm32f427VIT6 with a ZIT6 without changing the code?

Could get my hands on some ZIT6 instead of the almost unobtainable vit6 for free, but want to know if its possible without changing the software

This topic has been closed for replies.
TDK
TDKBest answer
Jul 27, 2021 4:09 PM UTC

Yes, the code will work without modification assuming your footprint is changed appropriately.

> They are compatible in pinout and no change is needed.

Not sure I'd call LQFP100 and LQFP144 compatible in pinout.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

ST Technical Moderator
Jul 27, 2021 4:07 PM UTC

Hello @DSmit.11​ ,

They are compatible in pinout and no change is needed in software.

You can use "Cross Selector" feature with STM32CubeMx tool to compare the characteristics (please see attached file comparing STM32F427VITx with STM32F427ZITx).

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
TDK
TDKBest answer
Jul 27, 2021 4:09 PM UTC

Yes, the code will work without modification assuming your footprint is changed appropriately.

> They are compatible in pinout and no change is needed.

Not sure I'd call LQFP100 and LQFP144 compatible in pinout.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
Jul 27, 2021 4:41 PM UTC

@TDK​ yes not fully compatible ;) I mean no position change from STM32F427VITx to F427ZITx.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
DSmit.111
DSmit.111Author
Associate
Jul 27, 2021 4:51 PM UTC

Hi imen,

I know that the zit6 had 44 PINS extra, therefore i need to change the PCB, but iwant to​ know if i can Just upload the code and it works if i connect alle in and outputs to the coresponding pins