Replace RTC Crystal with RTC Oscillator ?
We are working on a custom board based on STM32L476RGT6, and we are facing 32.768Khz crystal startup issue. Board stucks at the startup in following piece of code :
HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
and it fails while waiting for RCC_LSE_TIMEOUT_VALUE.
So after disabling this crystal, STM32 boots up fine.
We are using same crystal as in the NUCELO-L476RG board.
We need a solution to this problem, as this issue occasionally occurs in the nucelo board as well, which is very alarming. We have a target to ship 1k - 10k units to customer in an year and if we face these kind of issues, it will be impossible to debug these issues.
So my question is can i use a proper oscillator instead of this crystal ? If yes then what should be the specifications for that oscillator?
Thanks