Skip to main content
Associate III
Dec 23, 2024 9:12 AM UTC
Solved

Relationship between GPIO Interrupt and SPI Communication

We are trying to do SPI communication in the GPIO interrupt handler.
We are not sure about the following two points. Can someone please give me an answer?

1, If another GPIO interrupt occurs while the GPIO interrupt handler is running (with the same priority), does it wait for the GPIO interrupt handler running first to complete before running the later GPIO interrupt handler?
Or is the later GPIO interrupt ignored?

2,We would like to disable GPIO interrupts during SPI communication in order to perform SPI communication in the GPIO interrupt handler.
How should we write the program?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 23, 2024 10:08 AM UTC

@pass3master wrote:

Is there a way to prevent GPIO interrupts from occurring within an interrupt handler?


The interrupt does not occur within the interrupt handler. If it's the same IRQ handler it waits for the interrupt routine to finish and get back to it again. If another EXTI with higher preemption priority it will stop the execution of the lowest priority interrupt and execute the highest one.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

10 replies

Andrew Neil
Super User
Dec 23, 2024 9:14 AM UTC

Generally, doing any operation which takes a significant amount of time in an interrupt handler is a Bad Idea.

Why do you feel the need to do this?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
Dec 23, 2024 9:19 AM UTC

Oh, I see.

We are doing SPI communication (100μs) in the GPIO interrupt handler, but there is a possibility that the next GPIO interrupt comes in during SPI communication.

We are doing SPI communication in the GPIO interrupt handler.”
↑Is this idea wrong?

Andrew Neil
Super User
Dec 23, 2024 9:30 AM UTC

@pass3master wrote:

Is this idea wrong?


As I said, it's generally not a good approach.

Not enough detail to say whether you might just get away with it in your particular case.

Again, why do you feel the need to do the SPI comms within the interrupt handler?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
Dec 23, 2024 9:23 AM UTC

The EXTI pending bit is cleared as soon as the interrupt handler is executed:

void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)
{
 /* EXTI line interrupt detected */
 if(__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)
 {
 __HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);
 HAL_GPIO_EXTI_Callback(GPIO_Pin);
 }
}

Then the callback is called. So if in meantime (execution of the callback) an EXTI interrupt is fired, as soon as you exit the handler you will enter it again.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
Dec 23, 2024 9:57 AM UTC

Thank you for your answer.
I see. So when a GPIO interrupt occurs within an interrupt handler, it is put on hold and the handler is executed again immediately after it finishes.
Thank you. That's very helpful.
Is there a way to prevent GPIO interrupts from occurring within an interrupt handler?

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 23, 2024 10:08 AM UTC

@pass3master wrote:

Is there a way to prevent GPIO interrupts from occurring within an interrupt handler?


The interrupt does not occur within the interrupt handler. If it's the same IRQ handler it waits for the interrupt routine to finish and get back to it again. If another EXTI with higher preemption priority it will stop the execution of the lowest priority interrupt and execute the highest one.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.