Skip to main content
Visitor II
April 19, 2024
Question

Reinitialization of UART and ADC

  • April 19, 2024
  • 2 replies
  • 1283 views

Greetings,

I am trying to re- initialize the UART port  which i have already initalized with different settings. I Have used HAL_UART_DeInit() before initializing. The problem i face is after the function is run i see the same configuration which i removed.

i am facing similar issue on ADC peripheral when i configure and init different set of channel in different init function for same ADC.But i just see only one configration being used. I have used Deint () function for the ADC.

 

Kindly suggest me where i might be going wrong

 

Thank you!!

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
April 19, 2024

You're going to need to show the code you're using!

 

Please use this button to properly post source code:

AndrewNeil_0-1713523422399.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Aziz BRIGUI
ST Technical Moderator
May 20, 2024

Hello @sudhir467,

Welcome to ST Community !

To increase the chances of getting help from community users, perhaps you need to provide further details, part number used and code snippet as mentioned by @Andrew Neil.

Thanks,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.