Skip to main content
gaurav kumar
Associate II
June 3, 2017
Question

Regarding the state of CPU while DMA controller access bus for Data transaction.

  • June 3, 2017
  • 0 replies
  • 408 views
Posted on June 03, 2017 at 14:07

hi,

Is CPU halt when DMA access the bus for data transfer between peripheral and memory? if it is true then why in Application note  AN4031 they have written

''The DMA allows data transfers to take place in the background, without the intervention of

the Cortex-Mx processor. During this operation, the main processor can execute other tasks

and it is only interrupted when a whole data block is available for processing.'

because if CPU halts, then it doesn't matter whether CPU resources are free or not...

thanks 

#stm32f4 #dma #an4031
This topic has been closed for replies.