Skip to main content
NMuth
Associate
September 24, 2018
Question

Regarding the Interrupt

  • September 24, 2018
  • 0 replies
  • 501 views

i am working on enabling the gpio interrupt..i have setted a GPio pin as a interrupt and i have given priority for the interrupt and configured as a rising edge and written callback for that..

but the issue when i apply high on the GPIO the interrupt is not fired..

check the code.

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32l4xx_hal.h"
 
/* USER CODE BEGIN Includes */
#include<string.h>
/* USER CODE END Includes */
 
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef hlpuart1;
 
SPI_HandleTypeDef hspi1;
 
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
uint8_t transmit[20]="transmitter",receive[20];
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
static void MX_LPUART1_UART_Init(void);
 
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
 
/* USER CODE END PFP */
 
/* USER CODE BEGIN 0 */
void HAL_GPIO_EXTI_CALLBACK(uint16_t GPIO_pin)
{
	 HAL_SPI_StateTypeDef ret;
	 printf("\r\n intruppt \n\r");
	 while(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13) != GPIO_PIN_RESET);//
	if(GPIO_pin == GPIO_PIN_13)
	{
		printf("\r\ninside\n\r");
		memset(receive,'\0',sizeof(receive));
			 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
			 ret=HAL_SPI_GetState(&hspi1);
			 if(ret==HAL_SPI_STATE_READY)
			 {
				 HAL_SPI_TransmitReceive(&hspi1, (uint8_t*)transmit, (uint8_t *)receive, sizeof(transmit), 1000);
				 printf("\r \n received data:%s \n \r",receive);
				 HAL_Delay(200);
				 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
			 }
	}
 
}
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 *
 * @retval None
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration----------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_SPI1_Init();
 MX_LPUART1_UART_Init();
 /* USER CODE BEGIN 2 */
printf("\r \n SPI started \n \r");
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
while(1);
 
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 
 
 
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
 /* USER CODE END 3 */
 
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 
 RCC_OscInitTypeDef RCC_OscInitStruct;
 RCC_ClkInitTypeDef RCC_ClkInitStruct;
 RCC_PeriphCLKInitTypeDef PeriphClkInit;
 
 /**Configure the main internal regulator output voltage 
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 /**Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = 0;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
 RCC_OscInitStruct.PLL.PLLN = 60;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 /**Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_LPUART1;
 PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 /**Configure the Systick interrupt time 
 */
 HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
 
 /**Configure the Systick 
 */
 HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
 /* SysTick_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
 
/* LPUART1 init function */
static void MX_LPUART1_UART_Init(void)
{
 
 hlpuart1.Instance = LPUART1;
 hlpuart1.Init.BaudRate = 115200;
 hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
 hlpuart1.Init.StopBits = UART_STOPBITS_1;
 hlpuart1.Init.Parity = UART_PARITY_NONE;
 hlpuart1.Init.Mode = UART_MODE_TX_RX;
 hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 hlpuart1.FifoMode = UART_FIFOMODE_DISABLE;
 if (HAL_UART_Init(&hlpuart1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
}
 
/* SPI1 init function */
static void MX_SPI1_Init(void)
{
 
 /* SPI1 parameter configuration*/
 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_MASTER;
 hspi1.Init.Direction = SPI_DIRECTION_2LINES;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 7;
 hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
}
 
/** Configure pins as 
 * Analog 
 * Input 
 * Output
 * EVENT_OUT
 * EXTI
*/
static void MX_GPIO_Init(void)
{
 
 GPIO_InitTypeDef GPIO_InitStruct;
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();
 HAL_PWREx_EnableVddIO2();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
 
 /*Configure GPIO pin : PC13 */
 GPIO_InitStruct.Pin = GPIO_PIN_13;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 /*Configure GPIO pin : PA4 */
 GPIO_InitStruct.Pin = GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI15_10_IRQn, 1, 0);
 HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
 
}
 
/* USER CODE BEGIN 4 */
int _write(int file, char *ptr, int len)
{
	HAL_UART_Transmit(&hlpuart1,(uint8_t *)ptr,len,HAL_MAX_DELAY);
	return len;
}
 
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @param file: The file name as string.
 * @param line: The line in file as a number.
 * @retval None
 */
void _Error_Handler(char *file, int line)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 while(1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t* file, uint32_t line)
{ 
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/**
 * @}
 */
 
/**
 * @}
 */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

    This topic has been closed for replies.