Skip to main content
chowdaiah
Associate
July 24, 2014
Question

REGARDING STM32F030F4P6 GPIO configuration.

  • July 24, 2014
  • 7 replies
  • 1540 views
Posted on July 24, 2014 at 05:13

HI,

I have faced one problem with PORTF pin configuration (PF0,PF1).

My GPIO configuration:

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOF, ENABLE);

InitGpio.GPIO_Pin = (GPIO_Pin_0 | GPIO_Pin_1 );

InitGpio.GPIO_Mode = GPIO_Mode_AF;

InitGpio.GPIO_Speed = GPIO_Speed_Level_1;

InitGpio.GPIO_OType = GPIO_OType_PP;

InitGpio.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_Init(GPIOF, &InitGpio);

I am not getting any output from those PINs, if i tried normal GPIO configuration also. .

please suggest us is there any issue with that configuration.

Regards,

Chowdaiah

    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    July 24, 2014
    Posted on July 24, 2014 at 05:41

    Is this on a Discovery Board? Are there solder bridges related to getting these to header pins?

    /* GPIOF Periph clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOF, ENABLE);
    /* Configure PF0 and PF1 in output pushpull mode */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOF, &GPIO_InitStructure);

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    chowdaiah
    chowdaiahAuthor
    Associate
    July 24, 2014
    Posted on July 24, 2014 at 07:24

    it is not evaluation board , we have build for our small project purpose.

    zzdz2
    Associate
    July 24, 2014
    Posted on July 24, 2014 at 09:20

    Reference manual says these pins are special, looks like there is no point in configuring PF0/1 as alternate function.

    RM0360:

     

    8.3.13 Using the HSE or LSE oscillator pins as GPIOs

     

           When the HSE or LSE oscillator is switched OFF (default state after reset), the related

     

           oscillator pins can be used as normal GPIOs.

     

           When the HSE or LSE oscillator is switched ON (by setting the HSEON or LSEON bit in the

     

           RCC_CSR register) the oscillator takes control of its associated pins and the GPIO

     

           configuration of these pins has no effect.

     

           When the oscillator is configured in a user external clock mode, only the OSC_IN or

     

           OSC32_IN pin is reserved for clock input and the OSC_OUT or OSC32_OUT pin can still be

     

           used as normal GPIO.

     

     

    chowdaiah
    chowdaiahAuthor
    Associate
    July 24, 2014
    Posted on July 24, 2014 at 10:15

    I have already initialized same but it is not executed any output.

    zzdz2
    Associate
    July 24, 2014
    Posted on July 24, 2014 at 15:04

    I can set these pins to output without library:

    #include <stm32f0xx.h>
     
     RCC->AHBENR |= RCC_AHBENR_GPIOFEN;
    GPIOF->OTYPER = 0;
    GPIOF->OSPEEDR = 0;
    // PF0/1 output
    GPIOF->MODER = GPIO_MODER_MODER0_0 | GPIO_MODER_MODER1_0;
    // PF0/1 no pull
    GPIOF->PUPDR = 0;
    GPIOF->BSRR = GPIO_BSRR_BS_0 | GPIO_BSRR_BS_1;

    chowdaiah
    chowdaiahAuthor
    Associate
    July 25, 2014
    Posted on July 25, 2014 at 10:53

    I have tried this one also but it is not working.

    Tesla DeLorean
    Guru
    July 25, 2014
    Posted on July 25, 2014 at 15:10

    May be it's your board or chip, or how the chip is soldered. Do you have multiple boards exhibiting this problem? I don't have any TTSOP20 parts to evaluate.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..