Question
Receiving CANbus data
Posted on April 22, 2015 at 01:27
SO I am incredibly confused. I have an application that uses CANbus. I have the transmit running fine and I am to the point where I am receiving interrupts when I receive a message. so I am confused by the lack of documents, but can anyone tell me what the difference is between HAL_CAN_Receive_IT() and HAL_CAN_Receive()?
I have seen code samples with HAL_CAN_Receive in the ISR and I have seen HAL_CAN_Receive_IT in regular code. I am not sure how to get to the data when I am in the ISR. I have seen samples that look like this: CanRxMsgTypeDef RMess; RMess.FIFONumber = CAN_FIFO1; RMess.FMI = 14; RMess.StdId = 0x541; RMess.DLC = 0; RMess.RTR = 0; RMess.IDE = CAN_ID_STD; hcan2.pRxMsg = &RMess; HAL_CAN_Receive_IT(&hcan2,CAN_FIFO1); /* USER CODE BEGIN 3 */ /* Infinite loop */ while (1) I don't understand why I would want to pre-populate RMess if I am about to overwrite it with receive data. I already have a filter. Can someone please help me understand these APIs and how I get data after the interrupt arrives? BY the way -- I have a fully operational canbus and several nodes receiving the data and sending me data. I understand the transceivers and terminations. I can see the data arriving at the device with the scope and I am getting the interrupt when data arrives. Thanks Steve #c