Reading TIMx->DMAR from unrelated (channel/stream) DMA request
Hello,
I was looking for datasheets or specs or any other information from knowledgable people about reading a timer's DMAR register from a DMA request triggered by *another* timer. I was wondering how much reliable this design is, and if I should think about possible unwanted side effects. This is with a STM32F767, but I guess all the F series would share more or less the same design.
Here is a summary of my sofware design:
* TIM3->CH{1,2,3,4} input capture mode, 'free running' (TIM3->ARR = 0xffff to avoid wrapping), capturing both edges of 4 unrelated signals. The idea is to reliably 'timestamp' the edges of the input to later decode the signal etc.
* TIM8 periodic update (e.g. 1MHz) triggering appropriate DMA2 stream/channel on update.
* DMA2 configured as Periph->Mem, imporant detail is PBURST=INCR4, reading four times through TIM3->DMAR. TIM3->DCR configured with DBL=3 (4 transfers), DBA reading through TIM3->CCR{1,2,3,4}.
I came up with this design to avoid TIM3 wrapping and getting ambigous capture events (I cannot use DMA TIM3_CHx events because of the lack of available DMA channels on this particular hardware, so I must use either TIM3_UP for the 4 channels or a DMA2 channel, hence TIM8).
This works well. The only issue is that the TIM8 DMA request is triggered only once when reading TIM3->DMAR (thus not recognized as a burst by TIM3 nor TIM8). So I configured PBURST=INCR4 that makes the magic work in combination with TIM3->DBL=3, that cycles well through the 4 tranfers.
[Luckily I need exactly a INCR4. I also though of running TIM8 4 times faster and thus triggering 4 more transfers without PBURST.]
I also noticed that 'regular' reads (from code) through TIM3->DMAR happens to work too, i.e. each read cycles through the next address and proprely wraps after the 4 tranfers. What is a bit confusing in RM0410 about DMAR is that it's only mentionned about 'dma'.
My question is basically "how much is mixing DMA requests from one TIM event to DMAR of another TIM specified by the STM32 design" ...
Cheers,