Skip to main content
Lynn Linse
Associate III
Dec 12, 2016 3:23 PM UTC
Solved

reading STM32L15x program counter (with HAL defines?)

Posted on December 12, 2016 at 16:23

Question - What is the safest way to 'peek' at the STML152 program counter? Ideally something in the standard HAL files (so no ASM; I am working under AC6 in C). I wish my code to understand if it was loaded/is running in the lower 1 of 2 flash banks (? PC < 0x8004000), or in the upper 2 of 2 banks (PC > 0x8004000).

Background - this is a kind of dual boot issue, but not really. The L152 has 512K flash in 2 x 256K banks and we plan to load 2 similar images in the two 256K banks. We'll always boot from the lower bank image, but wish to load field fw upgrades into the upper bank image, understanding that the reflash might fail & need to be erased completely. The upper bank will be re-written by our own code (FW read from a special secure SPI token), and that loading code will be linked to load/run from the upper bank only.

The goal is to treat the lower bank as a 'factory default image', and the upper bank as a 'field written & perhaps broken image'. So we want a simple piece of code that basically does this IF test:

if(I am running in lower bank - aka: PC < X?)

  then I am factory image

      if(secure token is in place)

          consider reflash of upper FW - means one needs to power-cycle with secure token in place to reflash

      else

         examine upper image for validity (crc, maybe digital hash signature)

         if(upper image is valid)

             then jump to it & run

             else erase the invalid image & continue running the original factory image.

  else I am field image (PC > X?), so just run & don't bother looking for second/upper image or token

So the goal is to load new fw from the secure token, while running in the lower/factory image. I can completely erase the upper bank and attempt to write. We assume if the write is aborted, we'd end up with a partial/invalid image and the above test-for-validity could detect the bad FW status & erase it. We plan to use flash protection to disable the normal STLink reflash for field units (so one would need to erase all flash to re-enable such fw loading).

#dual-bank #nucleo-l152re #stm-registers
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 12, 2016 3:47 PM UTC
Posted on December 12, 2016 at 16:47

Not sure why everyone is afraid of assembler.

Something trivial that returns the link register, R0 is a return parameter, link

WhereAmI:

  mov r0, lr

  bx lr

uint32_t WhereAmI(void); // returns the caller return address

Or

extern void * __Vectors; // Keil

NVIC_SetVectorTable((u32)(&__Vectors), 0x0); // Smart Base Location

extern void * g_pfnVectors; // More GNU/GCC centric

NVIC_SetVectorTable((u32)(&g_pfnVectors), 0x0); // Smart Base Location

ie the address of the table tells you the basis.

Or think about how qsort() works, pointers to functions....

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 12, 2016 3:47 PM UTC
Posted on December 12, 2016 at 16:47

Not sure why everyone is afraid of assembler.

Something trivial that returns the link register, R0 is a return parameter, link

WhereAmI:

  mov r0, lr

  bx lr

uint32_t WhereAmI(void); // returns the caller return address

Or

extern void * __Vectors; // Keil

NVIC_SetVectorTable((u32)(&__Vectors), 0x0); // Smart Base Location

extern void * g_pfnVectors; // More GNU/GCC centric

NVIC_SetVectorTable((u32)(&g_pfnVectors), 0x0); // Smart Base Location

ie the address of the table tells you the basis.

Or think about how qsort() works, pointers to functions....

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Dec 12, 2016 3:51 PM UTC
Posted on December 12, 2016 at 16:51

Absolute addresses in the vector table tend to make truely position independent code a challenge.

Generally I'd have a small loader that doesn't get erased validate an image before jumping to it. If the flash write fails to complete the CRC doesn't resolve, if the write gets corrupted, the CRC also doesn't resolve. Mission Accomplished.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..