Skip to main content
baranovus
Associate III
June 12, 2024
Solved

Reading I2c with sub-address

Hello All.

Reading a register value from an I2C device assumes:  Writing the device address-> Writing the register address without STOP-> Reading the value . I am trying to figure out if I can do it using only available HAL functions but I don't see how. Simple Write followed by Read includes STOP, which is not in full compliant with the rules. 

Yes, if needed, I can rewrite everything but maybe there is an option, which I don't notice?

I use STM32G0B0 with HAL libraries.

 

This topic has been closed for replies.
baranovus
baranovusBest answer
Associate III
June 20, 2024

Thanks! That is the solution.

2 replies

Tesla DeLorean
Guru
June 12, 2024

For EEPROM, IMU, etc this form tends to be workable

HAL_StatusTypeDef status = HAL_I2C_Mem_Read(&I2CHandle, (0x42 << 1), 0xFF, 1, buffer, len, 300); // Read data block from register position 0xFF (8-bit)

Supports 8 and 16-bit addressing within the Slave, and whatever length auto-increments

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
baranovus
baranovusAuthorBest answer
Associate III
June 20, 2024

Thanks! That is the solution.