Reading flash and sending to UART
Hello,
I'm currently struggling to setup flash reading launched from a PC.
I've used the example code for simple write and read with HAL from STM32 Cube SW.
The example show a reading of an uint32_t after writing a uint64_t.
Here is my code:
Writing flash (byte array to uint64_t) . I use a uint8_t array [88] as a buffer for the datas I generate. So I slice this buffer 8 bytes everytime to create an uint64_t for the HAL_FLASH_WRITE function.
uint64_t mydata = 0;
uint8_t buffer_flash_ht[88] ;
uint8_t reglet = 0;
uint8_t tampon8[8];
for (uint8_t i = 0; i < 8; i++){
tampon8[i] = buffer_flash_ht[i + reglet];
}
reglet = reglet + 8;
for (int i=0; i<8; ++i){
mydata = (mydata << 8) | tampon8[i];
}
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, mydata) == HAL_OK)
{
Address = Address + 8;
}Reading flash
while (Address < FLASH_USER_END_ADDR){
data64 = *(__IO uint64_t *)Address;
uint8_t *message_data = (uint8_t *)&data64;
uint8_t result[8];
for(int i = 0; i < 8; i++) {
result[i] = message_data[i];
}
HAL_UART_Transmit(huart,message_data,sizeof(message_data),200);
Address = Address + 8;
}The datas I obtain from this algorithm don't make sense.
I should get (for example) a 'h' (0x68) char in first position. But I receive a 0x19. And none of the others bytes I get correspond to what I wrote first.
Did I made a mistake in my pointer/value operations? I'm still not very confortable with this kind of instruction.
Thank you.