Read/Write on a register
Hello, I'm having a trouble to read or write bits on registers, for example I would like to change the comparator input minus pin, according to the RM I have to change the INMSEL bits in the COMP1_CSR register, but when I write this line code:
COMP1_CSR = 0xF7854876 // just an examplethe IDE tells me that "COMP1_CSR is not declared", and it's the same thing with other registers, I cannot directly manipulate them...
I'm using STM32 Nucleo L476.