Skip to main content
Henry Brasil
Associate II
January 17, 2018
Question

Read-while-write (RWW) feature on the STM32F427IG doesn't work

Posted on January 17, 2018 at 18:11

Hello, I am using the STM32F427IG with 1MB of flash with the following configuration:

DB1M(dual bank mode) option byte ON

BFB2(run from bank2) option byte OFF

Looks like that when I write to the BANK2 with the following function the dual bank mode RWW(read while write) doesn't work, as the LED toggle inside the systick functions stop until the erase of some banks is over.

Where I am wrong ? I am running the code from the BANK1

  

I erase with the following function:

void eraseBank2Sectors{

  FLASH_EraseInitTypeDef EraseInitStruct;

  EraseInitStruct.TypeErase = TYPEERASE_SECTORS;

  EraseInitStruct.VoltageRange = VOLTAGE_RANGE_3;

  EraseInitStruct.Sector = FLASH_SECTOR_17;

  EraseInitStruct.NbSectors = 3;

  APP_Printf('BTL: FLASH erasing on bank2 sector 17,18,19...\n');

  if (HAL_FLASHEx_Erase_IT(&EraseInitStruct) != HAL_OK){

  APP_Printf('BTL: FLASH erase on bank2 FAIL \n');

}

and the systick handler as the following:

void SysTick_Handler(void)

{

HAL_IncTick();

GPIO_TOGGLE_UP_LED_HEARTBEAT();

HAL_SYSTICK_IRQHandler();

}
    This topic has been closed for replies.

    1 reply

    Henry Brasil
    Associate II
    January 18, 2018
    Posted on January 18, 2018 at 18:35

    Solved