Skip to main content
zizou_zaydoun1988
Associate
May 11, 2012
Question

Read state of pin STM32

  • May 11, 2012
  • 15 replies
  • 3565 views
Posted on May 11, 2012 at 15:28

HELLO,

I use

The

STM32L152RBT6

.

I want to know

how I can

read

the logic state

of a pine tree

if it is

up or down

and display it on

LCD. 

#!rocketscience
    This topic has been closed for replies.

    15 replies

    esiqueira
    Associate III
    May 11, 2012
    Posted on May 11, 2012 at 15:53

    /* Reads the pin(3) of the GPIOA and store it in ReadValue variable */

    u8 ReadValue;

    ReadValue = GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_3);

    esiqueira
    Associate III
    May 11, 2012
    Posted on May 11, 2012 at 15:54

    if (

    GPIO_ReadInputDataBit(GPIOA

    ,

    GPIO_Pin_3)==0)

    {

        [...code...]

    }

    LCD SPI?

    Tesla DeLorean
    Guru
    May 11, 2012
    Posted on May 11, 2012 at 16:21

    LCD SPI?

    Probably not, the STM32L152 can drive the simple glass on it's own.

    Not sure how the pine tree works, spruce or douglas?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    zizou_zaydoun1988
    Associate
    May 11, 2012
    Posted on May 11, 2012 at 16:26

    thank you very much

    ,

    but

    is it possible

    to give me

    the instruction to

    display the status

    of

    pine

    on the display

    LCD

    STM32

    board

    after

    reading it

    and

    thank you in advance

    esiqueira
    Associate III
    May 11, 2012
    Posted on May 11, 2012 at 16:32

    Sorry,

    Is this board???

    • STM32L152RBT6 microcontroller featuring 128 KB Flash, 16 KB RAM, 4 KB EEPROM, in an LQFP64 package

    • On-board ST-Link/V2 with selection mode switch to use the kit as a standalone ST-Link/V2 (with SWD connector for programming and debugging)

    • Board power supply: through USB bus or from an external 3.3 or 5 V supply voltage

    • External application power supply: 3 V and 5 V

    • IDD current measurement

    • LCD

      • DIP28 package

      • 24 segments, 4 commons

    • Four LEDs:

      • LD1 (red/green) for USB communication

      • LD2 (red) for 3.3 V power on

      • Two user LEDs, LD3 (green) and LD4 (blue)

    • Two pushbuttons (user and reset)

    • One linear touch sensor or four touchkeys

    • Extension header for LQFP64 I/Os for quick connection to prototyping board and easy probing

    • http://www.st.com/internet/evalboard/product/250990.jsp

      From: ayari.zied

    Posted: Friday, May 11, 2012 4:26 PM

    Subject: Read state of pin STM32

    thank you very much

    ,

    but

    is it possible

    to give me

    the instruction to

    display the status

    of

    pine

    on the display

    LCD

    STM32

    board

    after

    reading it

    and

    thank you in advance

    zizou_zaydoun1988
    Associate
    May 11, 2012
    Posted on May 11, 2012 at 16:46

    yes it is

    the same card

    as mine

    , so

    is

    that

    you can help me

    ?

    esiqueira
    Associate III
    May 11, 2012
    Posted on May 11, 2012 at 18:29

    I think you need reference the library: stm32l_discovery_lcd

    Then use this function to display message at LCD

    /* Display Welcome message */

    LCD_GLASS_ScrollSentence('' **PIN 3 ACTIVE**'',1,SCROLL_SPEED);

    This funcion can be found at: stm32l_discovery_lcd.c

    /**

    * @brief This function writes a char in the LCD RAM.

    * @param ptr: Pointer to string to display on the LCD Glass.

    * @retval None

    * @par Required preconditions: Char is ASCCI value ''Ored'' with decimal point or Column flag

    */

    void LCD_GLASS_DisplayStrDeci(uint16_t* ptr)

    {

    uint8_t i = 0x01;

    uint8_t char_tmp;

    // LCD_GLASS_Clear();

    /* Send the string character by character on lCD */

    while ((*ptr != 0) & (i < 8))

    {

    char_tmp = (*ptr) & 0x00ff;

    switch ((*ptr) & 0xf000)

    {

    case DOT:

    /* Display one character on LCD with decimal point */

    LCD_GLASS_WriteChar(&char_tmp, POINT_ON, COLUMN_OFF, i);

    break;

    case DOUBLE_DOT:

    /* Display one character on LCD with decimal point */

    LCD_GLASS_WriteChar(&char_tmp, POINT_OFF, COLUMN_ON, i);

    break;

    default:

    LCD_GLASS_WriteChar(&char_tmp, POINT_OFF, COLUMN_OFF, i);

    break;

    }

    /* Point on the next character */

    ptr++;

    /* Increment the character counter */

    i++;

    }

    }

    ________________

    Attachments :

    stm32l_discovery_lcd.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtDW&d=%2Fa%2F0X0000000aKO%2FFhSOtSxvdFAq6DUKhYrE6hnMtwnlFnyWftoSsjUTpB8&asPdf=false

    stm32l_discovery_lcd.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtVt&d=%2Fa%2F0X0000000aR6%2FUs8_tSilfLoz7gyKUumW5SKx._7_RWoGFoSo66gJn3Q&asPdf=false
    zizou_zaydoun1988
    Associate
    May 14, 2012
    Posted on May 14, 2012 at 10:53

    Again, thank you

    ,

    but I want

    the instruction that

    allows me to send

    the logic state of 

    pin

    PA3 for

    example

    to

    LCD

    Tesla DeLorean
    Guru
    May 14, 2012
    Posted on May 14, 2012 at 19:48

    Again, thank you

    ,

    but I want

    the instruction that

    allows me to send

    the logic state of

    pin

    PA3 for

    example

    to

    LCD

    if (GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_3)==0)
    LCD_GLASS_DisplayString(''PA3 LOW'');
    else
    LCD_GLASS_DisplayString(''PA3 HIGH'');

    Perhaps you need to review some of the example code for the STM32L Discovery board and get more familiar with programming
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    zizou_zaydoun1988
    Associate
    May 15, 2012
    Posted on May 15, 2012 at 10:50

    I tried

    to

    connect the

    PA3

    pin

    to pin

    VDD and

    sometimes

    PIN 

    3V

     

    but

    LCD

    still

     

    displays

    ''LOW''

    , I

    do not know why

    :

    (