Skip to main content
Ivchenko Dmytro
Associate
Jun 20, 2017 2:41 PM UTC
Question

read gps data on stm32f103

Posted on June 20, 2017 at 16:41

Hello dear ST programmer!

At least one month I`m trying to implement gps neo-6m module with my inemo-discovery board and I really get nothing, i have already implemented altimeter and it is works good now I need to read gps data. If someone can help me I will be pleased.

please help me.

    This topic has been closed for replies.

    6 replies

    Tesla DeLorean
    Guru
    Jun 20, 2017 3:13 PM UTC
    Posted on June 20, 2017 at 17:13

    The NEO-6M should output NMEA sentences at 9600 8N1 via it's TX pin into an STM32 USART RX pin.

    >> I really get nothing

    Not really very illuminating about what your code is doing, how and to what the connectivity is implemented.

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Ivchenko Dmytro
    Associate
    Jun 20, 2017 8:48 PM UTC
    Posted on June 20, 2017 at 20:48

    Thanks for your prompt respond.

    The main idea to implement program using ChibiOS for iNemo-Discovery board to read data from 

    internal(thermometer, barometer and pressure sensor) and 

    external(altimeter and GPS).

    I have already implemented all of them except GPS, because I really have no idea how to do this using ChibiOS.

    Self.Glenn
    Visitor II
    Jun 21, 2017 1:51 AM UTC
    Posted on June 21, 2017 at 03:51

    Here's a demo project for the stm32f103.

    If you use it with an rtos, you should probably send back data through a queue from the ISR to a receiving task.

    The demo uses the nmea library that can be found here:

    https://sourceforge.net/projects/nmea/

    Demo project is here:

    http://glennsprojects.com/download/zipfiles/gps_demo.zip

     

    Hope this helps

    Glenn

    Ivchenko Dmytro
    Associate
    Jun 21, 2017 2:20 PM UTC
    Posted on June 21, 2017 at 14:20

    Thanks for your respond.

    I will try to implement according to your demo project.

    Thank you☺

    Andrei Chichak
    Lead
    Jun 21, 2017 2:09 AM UTC
    Posted on June 21, 2017 at 04:09

    Have you ever read any data on your serial port? Even loopback?

    Are you using C? Are you using stdio functions? Have you written the shim to connect the UART into the stdio functions?

    Which compiler are you using? Which toolset?

    So many questions.

    Andrei from The Great White North

    see 

    http://embedded.fm/blog/2016/11/29/discovery-uarts-part-1

     
    Ivchenko Dmytro
    Associate
    Jun 21, 2017 2:43 PM UTC
    Posted on June 21, 2017 at 14:43

    Dear Mr Andrei,

    Thanks for your respond.

    Yes I have. I can read data(Temperature and Atmospheric pressure) on my serial port using terminal window.

    I am using 'C', Chibi Studio 17 based on Eclipse 'Luna'

    Code that I already implemented 

    https://www.dropbox.com/sh/6zbr6wwdh45taie/AADxixZr70yRbrR2xVE5yEtna?dl=0

    Thank you☺