Skip to main content
jiaqi zhao
Associate
May 18, 2017
Question

Re: F429 Serial Audio Interface hardware examples?

Posted on May 18, 2017 at 10:45

Hi,

I have  a project that i need to make a 7 microphone array. I want to use SAI  with TDM, but I can't find any exemple. Did you solve your problem? Can you give me some suggestions?

Thanks

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    May 18, 2017
    Posted on May 18, 2017 at 11:37

    Hi

    zhao.jiaqi

    ,

    Try thisSAI example based on the STM324x9I_EVAL

    board under

    STM32CubeF4 V4.0:

    STM32Cube_FW_F4_V1.0\Projects\STM324x9I_EVAL\Examples\SAI\SAI_Audio

    Since, this example provides basic implementation of audio features on the STM324x9I_EVAL boardusing the external codec WM8994 andsupporting the TDM format.

    Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks