Skip to main content
flyer31
Senior
March 28, 2013
Question

RCC_CFGR_HRPE Bit? (SysClk Devider)

  • March 28, 2013
  • 3 replies
  • 739 views
Posted on March 28, 2013 at 10:12

Hi,

in the file System_ST32F4xx.c of the ST4Discovery examples, I always find the following 2 lines for the clock configuration (SysClk 168MHz):

    /* HCLK = SYSCLK / 1*/

    RCC->CFGR |= RCC_CFGR_HPRE_DIV1;

      

    /* PCLK2 = HCLK / 2*/

    RCC->CFGR |= RCC_CFGR_PPRE2_DIV2;

    

    /* PCLK1 = HCLK / 4*/

    RCC->CFGR |= RCC_CFGR_PPRE1_DIV4;

I understand the meaning for the last 4 lines - here SysClk must be devided by 2 or 4, resp., as the APB1 and APB2 frequencies are limited to 84MHz and 42MHz.

But concerning the first 2 lines, here the RM 6.3.3(RCC_CFGR) states:

Bits 7:4 HPRE: AHB prescaler

Set and cleared by software to control AHB clock division factor. ...

0xxx: system clock not divided

1000: system clock divided by 2

...

So according to this register description, RCC_CFGR_HRPE could be left on its init value of 0. Why is it programmed to the value ''2'' in the ST4Discovery examples? Anyone has any idea?

    This topic has been closed for replies.

    3 replies

    waclawek.jan
    Super User
    March 28, 2013
    Posted on March 28, 2013 at 12:25

    I'd guess that they are autogenerated or simply product of copy/paste. Take it as a template for your code where you might potentially want to use a different divider.

    > Why is it programmed to the value ''2'' in the ST4Discovery examples?

    In my copy of stm32f4xx.h:

    #define  RCC_CFGR_HPRE_DIV1                  ((uint32_t)0x00000000)        /*!< SYSCLK not divided */

    Where do you have ''2'' from?

    JW

    flyer31
    flyer31Author
    Senior
    March 28, 2013
    Posted on March 28, 2013 at 16:30

    Thank you for your answer.

    The command

    RCC->CFGR |= RCC_CFGR_HPRE_DIV1

    puts HPRE to ''2'' (as DIV1 is the 2nd bit in this HPRE field).

    waclawek.jan
    Super User
    March 28, 2013
    Posted on March 28, 2013 at 16:52

    No. The C compiler doesn't know about what is written in reference manual.

    Check how 

    RCC_CFGR_HPRE_DIV1

    is defined in the library files you are including/linking. Chances are, that it's a macro defined as I described above.

    JW

    [EDIT] Oh, I now see what's the source of your confusion:

    #define  RCC_CFGR_HPRE_1                     ((uint32_t)0x00000020)        /*!< Bit 1 */

    versus

    #define  RCC_CFGR_HPRE_DIV1                  ((uint32_t)0x00000000)        /*!< SYSCLK not divided */

    Oдна буква и кака�? разница... ;)

    JW