Skip to main content
ADevi.1
Associate
Mar 17, 2020 4:08 AM UTC
Question

RC Radio PWM signal, problems reading

Hi,

Im trying to resurrect this project from 2015 (Software AWD control for RC Cards using 4x brushless motors):

https://github.com/hammerfet/BrinirController

Ive built his VS2013 solution and got all that side working fine. However, next is to determine I can read the RC Radio signal (standard RC drone Turnigy 9x and FRSky V8FR-II receiver) and Im getting problems. The signals are just two, throttle and steering and connected to PA0 and PA1 on a STM32 F407 discovery.

Sometimes it doesnt read anything, sometimes it reads it once occasionally it reads everything fine.

Here is the IO code:

/* TIM2 Init - PPM Inputs */

htim2.Instance = TIM2;

htim2.Init.Prescaler = PPMMEASUREPRESCALER;

htim2.Init.CounterMode = TIM_COUNTERMODE_UP;

htim2.Init.Period = 65535;

htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

HAL_TIM_Base_Init(&htim2);

sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig);

sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig);

HAL_TIM_Base_Start_IT(&htim2);

and some more references in config.h:

  #define PPMMEASUREPRESCALER 4

  #define RECEIVERMINSIGNAL 500

  #define RECEIVERMIDSIGNAL 25000

  #define RECEIVERMAXSIGNAL 34000

Is there anything obviously wrong here? Anything I should know about connecting RC Radio PWM to the F407?

This topic has been closed for replies.

9 replies

waclawek.jan
Super User
Mar 17, 2020 6:19 AM UTC

Timers have a PWM input "mode" - use it. Read the timer chapter in RM.

JW

ADevi.1
ADevi.1Author
Associate
Mar 21, 2020 9:31 AM UTC

Right, read the chapter, looked at the code and tried every combo of modes.

Here is the default:

GPIO_InitStruct.Pin = REC1PIN | REC2PIN | FB1PIN | FB2PIN | FB3PIN | FB4PIN;

GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;

GPIO_InitStruct.Pull = GPIO_PULLUP;

HAL_GPIO_Init(RECPORT/*same as FBPORT*/, &GPIO_InitStruct);

REC1 and 2 are PA0 and PA1 on TIM2.

As I said, it works sometimes (5% of the time) and when its displaying anything than zero it seems to just capture the first reading then stops.. but again not 100% of the time. Is there a time out or something?

Piranha
Principal III
Mar 22, 2020 4:50 AM UTC

Well, now read the GPIO chapter, especially the alternate function configuration. =)

waclawek.jan
Super User
Mar 21, 2020 10:49 AM UTC

I don't understand what exactly you do and I don't use Cube, but maybe you should try to adopt the example from [STM32Cube_FW_F4_Vxxxx]\Projects\STM32F4-Discovery\Examples\TIM\TIM_PWMInput\

JW