Skip to main content
Raahul Jagannathan
Associate III
Jun 14, 2018 5:38 AM UTC
Question

Range of frequency counter is being limited. Why?

Posted on June 14, 2018 at 07:38

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    9 replies

    waclawek.jan
    Super User
    Jun 14, 2018 7:59 AM UTC
    Posted on June 14, 2018 at 09:59

    If I understand correctly, you are trying to count pulses of  the measured signal in TIM2, gated by TIM21, set to 1 second period, correct?

    As TIM2 is 16-bit only in 'L0, this cannot work higher than up to 65.535kHz. The demo you are mentioning, hasn't it been demonstrated on a different STM32 model?

    You have to change your approach. There are many ways to do that. One of them is described here:

    https://community.st.com/0D50X00009bMMA8SAO

     

    JW

    Raahul Jagannathan
    Associate III
    Jun 14, 2018 10:16 AM UTC
    Posted on June 14, 2018 at 10:16

    Thank you so much for the response. I know that the counter is only 16-bit. I can measure proper values upto 65KHz. After this, my OLED display shows me the overflow. This continues upto 72Khz. After this value, the frequency directly goes to 0. It does not record anything. That is what is confusing me.