Skip to main content
Associate
Apr 21, 2025 9:20 PM UTC
Solved

Random interrupts when an external interrupt trigger occurs

I'm generating external interrupts on an WeActStudio STM32F446RET6 board. I've the pins configured as pull-up. When I set one of them to GND, several random interrupts from other pins are generated. For example, if I connect pin PB3 to GND, I get interrupts from PB3 and PB4.

I attach the complete project, I'm compiling it with Visual Studio Code.

What could be the cause?

 

My callback function is:

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
 static uint32_t last_interrupt_time[6] = {0}; // For multiples pins
 uint32_t current_time = HAL_GetTick();
 #define debounce_time 50 //ms

 switch(GPIO_Pin) {
 case GPIO_PIN_0:
 if (current_time - last_interrupt_time[0] > debounce_time) {
 last_interrupt_time[0] = current_time;
 printf("INT PB0\r\n");
 } 
 break;
 case GPIO_PIN_1:
 if (current_time - last_interrupt_time[1] > debounce_time) {
 last_interrupt_time[1] = current_time;
 printf("INT PB1\r\n");
 } 
 break;
 case GPIO_PIN_3:
 if (current_time - last_interrupt_time[2] > debounce_time) {
 last_interrupt_time[2] = current_time;
 printf("INT PB3\r\n");
 } 
 break;
 case GPIO_PIN_4:
 if (current_time - last_interrupt_time[3] > debounce_time) {
 last_interrupt_time[3] = current_time;
 printf("INT PB4\r\n");
 } 
 break;
 case GPIO_PIN_5:
 if (current_time - last_interrupt_time[4] > debounce_time) {
 last_interrupt_time[4] = current_time;
 printf("INT PB5\r\n");
 } 
 break;
 case GPIO_PIN_6:
 if (current_time - last_interrupt_time[5] > debounce_time) {
 last_interrupt_time[5] = current_time;
 printf("INT PC6\r\n");
 } 
 break;
 default: break;
 }
}

 

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 21, 2025 9:24 PM UTC

Several EXTI dump into the same Handler?

HAL dispatchs in a shot-gun method rather than qualifying?

You've got noise or signal bounce on your inputs?

TIM pins in input capture might provide additional filter and clock options. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 21, 2025 9:24 PM UTC

Several EXTI dump into the same Handler?

HAL dispatchs in a shot-gun method rather than qualifying?

You've got noise or signal bounce on your inputs?

TIM pins in input capture might provide additional filter and clock options. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
juanjAuthor
Associate
Apr 22, 2025 6:08 AM UTC

Shared EXTI Handlers: Yes, I’m aware that EXTI9_5 shares one handler (for pins 5-9), but my issue also occurs with PB3 (EXTI3) and PB4 (EXTI4), which have dedicated handlers (EXTI3_IRQHandler/EXTI4_IRQHandler).

Noise/Bouncing: I already had software debounce implemented (50ms delay in callbacks), I've now added hardware debouncing (1kΩ series resistor + 100nF capacitor to GND) on a pin. It works! I didn't know that noise on a single pin can trigger interrupts on other pins.