Skip to main content
Davide Michelis
Associate II
May 18, 2018 12:54 PM UTC
Solved

RAM sections, map file, RAM memory filling

Posted on May 18, 2018 at 14:54

Good morning,

I am developing an application that uses STM32F3DISCO as board and FreeRTOS as OS. I want to keep some data in the RAM after some Software reset that I do under some conditions so I have used the notation

__attribute__((section('.my_section')))

near the variables I want to preserve. Moreover in the linker script I have added a section just after .data and before .bss

.my_section (NOLOAD):

  {

    . = ALIGN(4);

    _s_my_section = .;      

    *(.my_section)

    . = ALIGN(4) ;

    _e_my_section = .;

  } > RAM

Now, the application works correctly and the values are preserved but I want to understand more:

when I do a reset pressing the button I get my values stored  -> OK

when I do a power on reset values are more or less random -> OK

To put a 0 in those locations again I have to upload a program without that section defined...is the SRAM reset to 0 when a new .bin is flashed? Because otherwise I cannot explain this behavior.

Sorry if the question could seem a bit naive.

Greetings,

Davide

#soft-reset #memory-sections #ld-script #linker
    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    May 18, 2018 4:22 PM UTC
    Posted on May 18, 2018 at 16:22

    I'd probably lean toward putting this kind of data in the top of RAM, and shrinking the memory described to the linker. Or use the BKPRAM/NVRAM if available. On the F3 the 16KB of CCMRAM might be less vulnerable to use by the tools.

    >>Uhm ok thanks, so how can I be sure that I'm going to reset the region I will use to store/update those data across resets? 

    Storage structure has a leading signature, and trailing checksum/crc, this will fail a simple integrity check across the power-up scenario.

    typedef struct _FOORAMSTRUCT {

    uint32_t Sig;

    uint32_t Foo;

    uint32_t Bar;

    uint32_t Crc;

    } FOORAMSTRUCT;

    FOORAMSRUCT *ramstuff = (FOORAMSRUCT *)0x10000000;

    if ((ramstuff->Sig == 0xCAFECAFE) && (Crc32(0xFFFFFFFF, ramstuff, sizeof(FOORAMSTRUCT)) == 0)

    {

      // Structure Intact

    }

    else

    {

    // Structure Corrupt - copy in new defaults and sign

    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    6 replies

    Tesla DeLorean
    Guru
    May 18, 2018 1:12 PM UTC
    Posted on May 18, 2018 at 15:12

    The download process usually puts a loader into RAM, and that uses other areas of RAM to perform the FLASH Erase/Write operations.

    If you leave persistent data in RAM you might want to consider placing that all within a structure, and then having signatures and checksums so you can verify the integrity of that data, and copy in some new defaults when there is no valid data there.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Davide Michelis
    Associate II
    May 18, 2018 3:48 PM UTC
    Posted on May 18, 2018 at 15:48

    Uhm ok thanks, so how can I be sure that I'm going to reset the region I will use to store/update those data across resets? 

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    May 18, 2018 4:22 PM UTC
    Posted on May 18, 2018 at 16:22

    I'd probably lean toward putting this kind of data in the top of RAM, and shrinking the memory described to the linker. Or use the BKPRAM/NVRAM if available. On the F3 the 16KB of CCMRAM might be less vulnerable to use by the tools.

    >>Uhm ok thanks, so how can I be sure that I'm going to reset the region I will use to store/update those data across resets? 

    Storage structure has a leading signature, and trailing checksum/crc, this will fail a simple integrity check across the power-up scenario.

    typedef struct _FOORAMSTRUCT {

    uint32_t Sig;

    uint32_t Foo;

    uint32_t Bar;

    uint32_t Crc;

    } FOORAMSTRUCT;

    FOORAMSRUCT *ramstuff = (FOORAMSRUCT *)0x10000000;

    if ((ramstuff->Sig == 0xCAFECAFE) && (Crc32(0xFFFFFFFF, ramstuff, sizeof(FOORAMSTRUCT)) == 0)

    {

      // Structure Intact

    }

    else

    {

    // Structure Corrupt - copy in new defaults and sign

    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..