Skip to main content
russ
Associate III
September 22, 2008
Question

Quick reset and bootload question

  • September 22, 2008
  • 6 replies
  • 938 views
Posted on September 22, 2008 at 08:24

Quick reset and bootload question

    This topic has been closed for replies.

    6 replies

    russ
    russAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    Seriously? No one knows the answer to this?

    russ
    russAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    If I am not utilizing the manual reset input on the processor should I add a pull up resistor on that pin?

    Likewise, I am bootloading this processor. Do I need to apply a pull-down resistor on BOOT1 (note: not BOOT0) or can I leave it unconnected?

    Thanks in advance.

    tibo
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    The NRST pin has an internal pull up resistor with 40K, so I suppose that a pull up

    is not necessary (see page 86 in HD Datasheet). The reference design in AN2586

    has also no pull up.

    If you use only flash memory, I suppose you can use BOOT1 a normal GPIO

    (BOOT1 is shared with PB2).

    paul
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    I found that a pull-up was required on the reset line, the micro would not boot without it.

    I am not sure about the BOOT1 pull-down, I have one on my board.

    russ
    russAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    Tibo, you are right, but what Paul.Archer said worries me. Any second opinions?

    stevemelnikoff9
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    We have pull-downs on BOOT0 and BOOT1, and a pull-up on !RESET.