Question
Queue with uart for Nucleo L053-R8
Posted on September 29, 2014 at 23:44
Hi,
I'm a using a Nucleo L053-R8 board and i'm trying to implement a STR system. I'm using CMSIS RTX. And i want to implement a queue in RTX with a peripheral in reception mode(uart) . I started with creating a projet without RTX. And i implemeted my uart like this :char GetChar(void){
char a;
if(HAL_UART_Receive_IT(&huart1, (uint8_t*)aRxBuffer, 1)!= HAL_OK)
{
while(1){}
}
/*##-5- Wait for the end of the transfer ###################################*/
while (UartReady != SET)
{
}
/* Reset transmission flag */
UartReady = RESET;
a=aRxBuffer[0];
return a;
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{
/* Set transmission flag: trasfer complete*/
UartReady = SET;
}
with the IRQ declared like this
void USART1_IRQHandler(void)
{
HAL_NVIC_ClearPendingIRQ(USART1_IRQn);
HAL_UART_IRQHandler(&huart1);
} It worked perfectly!
i want to work in real time using rtx, so i trying to used a queue.
a = osPoolAlloc(mpool);
a[0]= aRxBuffer[0];
osMessagePut(MsgBox1, a[0], osWaitForever);
But i don't really know where i need to put the code to fill my queue.
I used to work a lot with FreeRTOS and i could do :
xQueueSendFromISR( xQueueRxUart, &tmp, &xHigherPriorityTaskWoken ); With this ''
xQueueSendFromISR'' in the uart ISR.
But i don't found an equivalent method with RTX.
Anyone knows how i can implement a queue in RTX with a peripheral in reception mode ?
Thanks you a lot. :)