Skip to main content
Dimitris Paraskevopoulos
Associate III
October 2, 2017
Question

Questions about UART_TwoBoards_ComIT example in STM32 Examples

Posted on October 02, 2017 at 14:59

I will focus my question on the receiver board to make it simpler.

In the example we are resetting a global flag and then requesting to receive some bytes. Then we wait until the HAL_UART_RxCpltCallback sets the flag while potentially doing some work instead of just waiting for the data as is done in the polling example (synchronous). When we receive the data we echo back the received data.

First of all I want to verify that the example as it currently is is essentially a synchronous operation if we do not add any code to the  while (UartReady != SET) loop.

I would like to know if this asynchronous + polling to see if the global variable has been set is the best way (Least amount of time spent not doing any meaningful work) to do this asynchronous communication.

Isn't this polling wasting CPU resources? Is there a different way to do this?

If I wanted to have a simple system where receiver receives some data processes them and returns back then should the pseudocode be:

while(1){

   HAL_UART_Receive_IT

   while (UartReady != SET) {

      process_data

   }

   UartReady = RESET;

   HAL_UART_Transmit_IT

   while (UartReady != SET){

      process_data

   }

}

So basically whenever we are not doing work on receiving or transmitting we are processing the data.

Is there a design pattern for this? If so how is it called.

Should we queue the next transmission whenever we receive some data i.e. in HAL_UART_RxCpltCallback along with setting the UartReady flag?

#stm32 #uart-it #asynchronous
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
October 2, 2017
Posted on October 02, 2017 at 15:57

I would generally look to doing receive and transmit in parallel as you really can't control when data will be received, and if not handled in a timely fashion will result in overruns and data loss.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Dimitris Paraskevopoulos
Associate III
October 2, 2017
Posted on October 02, 2017 at 16:21

Not entirely sure what you mean by doing it in parallel.

Do you suggest using SPI instead? Could you give an example or even better give pseudocode?

Cheers Clive.

Tesla DeLorean
Guru
October 2, 2017
Posted on October 02, 2017 at 16:45

Parallel, ie concurrently, not blocking Wait for A, Wait for B

while(1)

{

  if (RxIdle) HAL_UART_Receive_IT;

  if (TxIdle) HAL_UART_Transmit_IT;

 if (RxReady) ProcessRx;

 if (TxReady) ProcessTx;

 ProcessPump;

}

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..